cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 TSC Assert Failed. Default config unsupported?

EHyld.1
Associate II

Hello. I have set up TSC using the standard CubeMX config on Group 2 and 3, where the sampling is connected to G3_IO1 and G2_IO1. However, when i run the program, i get an assertion failure at the initialization on assert_param(IS_GPIO_AF_INSTANCE(GPIOx)); It seems the GPIOC port where is G3_IO1 connected to does not support Alternate Functions.

Here's the code the assertion does:

#define IS_GPIO_AF_INSTANCE(INSTANCE)   (((INSTANCE) == GPIOA) ||                                 ((INSTANCE) == GPIOB))

Here's a repo that reproduces the error: https://github.com/hyldmo/tsc-test. I used CubeMX 6.0.1 (and have seen the same on previous versions as well)

However, it seems like the touch works decently. Is this something i should be concerned about?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
EHyld.1
Associate II

Anyone has any ideas?