cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F205VGTx - Need support to enable the USB OTG High speed Dual role using the STM32CubeMx V5.6.1

DA.1115
Associate II

Hi all, Thanks for the support. I am using STM32CubeMx V5.6.1 to generate the driver for STM32F205VGTx USB OTG High speed dual role function.

I required USB OTG High speed for communication between to STM32 controller. So I am trying to enable using the STM32CubeMx V5.6.1. But I see WARNING as "This IP has no parameter to be configured"(Refer Image attached).

  1. Why the WARNING is shown?
  2. What is the impact due to this WARNING?

Thanks for sharing the experience.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MBugl.2
Associate

This should not be a problem.

The real problem is the Middleware USB_HOST and USM_DEVICE disabled.

Reading other old questions (2015 https://community.st.com/s/question/0D50X00009XkgMdSAJ/mx-usb-and-host-vs-device-support) I think the only solution is a DIY approach.

During last 5 years no improvements from ST on this?

(I asked my FAE but I got no answer)