2020-11-19 8:39 AM
I am pretty sure that old versions of CubeMX (maybe years ago), when generating for TCM interface generated different code than when generating for AXI.
At least in the generated STM32F765VGTx_FLASH.ld (I'm working with a F765), I had a base flash address of 0x200000 for ITCM and 0x8000000 for AXI, the #define FLASH_BASE was set accordingly and I had some code section in which the interface was set.
Now I am working with CubeMX 6.1.0 (the same for 6.0.1) and I notice that nothing changes in the code when I set TCM rather than AXI. The code seems to setup the AXI interface even when I set TCM.
Whats happened?
2020-11-20 12:20 AM
Dear @raffin ,
Thank you for your feedback.
Could you please share .ioc file ?
Kind regards,
Houssem
2020-11-20 2:00 AM
Dear Houssem,
thank you for the answer. Today I generated again several times using TCM and AXI. Now, I see the difference in the STM32F765VGTx_FLASH.ld file, I am sure yesterday this file did not change, in any the right address in the STM32F765VGTx_FLASH.ld it is not enough to set the TCM interface.
I have attached the .ioc file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.