STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1598 Views
  • 0 replies
  • 2 kudos

Resolved! Method to reorder peripheral init functions? (DMA BUG)

Is there a way to reorder the peripheral initialization functions in the main.c auto code without opening the .ioc file? MX_DMA_Init() was getting called after MX_USART1_UART_Init() in my project, which was causing the DMA instance's registers to not...

ALars.2 by Associate II
  • 1557 Views
  • 2 replies
  • 0 kudos

Resolved! cubeMX 6.4 dialog box breaks command line build

HelloVersion 6.4.0 (and maybe some versions before) introduces an ugly dialog box when generating code. This dialog box breaks command line generation because it needs somebody to click.Can it be replaced by a warning in the logs?ThanksJulien

JulienD by Senior
  • 2113 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE v1.8 generation error

/** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0};   /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABL...

ivainc by Associate III
  • 2132 Views
  • 3 replies
  • 0 kudos

Incorrect code generation for PLL of F767

I want to use HSI, not external component to generate frequency. I generate code by CubeIDE only (pack 1.16.1), there is no my code. I only add define USE_FULL_ASSERT and implement void assert_failed. But CubeIDE's code fails on assert_param(IS_RCC_P...

0693W000008xivuQAA.png 0693W000008xiw4QAA.png

CubeIDE strange build behaviour

I know, it's not easy to get this answer this way. I have a working F446RE code with CubeMX generated base in CubeIDE. I use the LL drivers and just simple int and string variables, not any dynamic memory handling. In some cases if I insert a new cod...

Peterb by Associate
  • 2337 Views
  • 5 replies
  • 0 kudos

Resolved! SAI slot number bug in CubeMX 6.4.0

Datasheet claims that with FSDEF=0 (FS signal is start frame, not channel identificaion) i can set up number of slots (NSBLOT) to any value. In my case 1. CubeMX claims that it must be equal two (which is not true). When i try to set value to 1, then...

stm32h7b0vb ADC+dma always Overrun Error

ADC Trigger from Timer,DMA transmit ,and then Always Overrun Error, buffer address @0x30000000.Data can not be transferred to buffer correctly,ADC1 register DR is 0x801 while buffer is 0x01.

0693W00000HpnN9QAJ.png
wjun.1 by Associate
  • 1894 Views
  • 3 replies
  • 0 kudos

Resolved! Simple ADC configuration - STM32G0 specific problem

Porting a working solution from STM32L031 to STM32G0B1 I try to configure ADC in CubeMX . It is a very simple, typical setup. 3 channels converted in "one shot" mode with DMA, triggered by slow 1Hz timer.All I am getting is HAL_ADC_ErrorCallback(), s...

0693W00000Hq3SUQAZ.png 0693W00000Hq3SZQAZ.png 0693W00000Hq3WMQAZ.png 0693W00000Hq3WHQAZ.png
TDJ by Lead
  • 3074 Views
  • 3 replies
  • 0 kudos