STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

stm32f769i-disco + FreeRTOS + Lwip + CubeMX: is it possible to produce an .ioc configuration with working ethernet?

Does somebody can provide a cubeMX generated file with working ethernet and freeRtos?? Is it even possible? I know there is a working example application but it is not from CubeMX. Using the new HAL eth driver from the F7 package I am not able to eve...

redmig by Associate III
  • 1613 Views
  • 2 replies
  • 0 kudos

Bug on the "HAL_PWREx_EnableWakeUpPin" function on STM32H7

Hello,I am using STM32H7B0VBT6 and I wanted to activate the wake up from Standby on PA0 (WAKEUP_PIN1) with rising edge, the code used is the following:PWREx_WakeupPinTypeDef sPinParams = {0};sPinParams.WakeUpPin = PWR_WAKEUP_PIN1;sPinParams.PinPolari...

cb.7 by Associate III
  • 939 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F4 HAL ETH broken

I have tried to generate a new project using STM32CubeIDE from scratch (fw V1.27.0, no way to modify it[!!!]) but it does not compile.A lot of descriptors are missing, like there is no resolution for the following:ETH_TxPacketConfig TxConfig; ETH_DMA...

VaZso by Associate III
  • 6007 Views
  • 8 replies
  • 1 kudos

Resolved! Error MX generation USART/DMA with STM32G0B

Hello community,Warning, when gerating code for STM32G0B with FW_1.5.0, DMA init function is called after USART2 init function.So the DMA doesn't works !!The only way to resolve this i have found is to cut/paste function in the good order ^^Report th...

tvill.1 by Associate II
  • 2353 Views
  • 5 replies
  • 0 kudos

How do I load an earlier version of the MX program? The current version does not generate code right like the previous version did.

I have been using the DMA for UART transmit for months without problem. The MX program is not generating the code for DMA configuration anymore. It used to work. I have other problems with the current version and I am tired of all the "it will be fi...

KiptonM by Lead
  • 2113 Views
  • 4 replies
  • 0 kudos

Why can't I download firmware package?

Hello. When I tried to use Motor Control Bench for the first time in a while, I had trouble downloading the firmware package.Looking at the log file at the time of code generation, the code appears to be generated.Do you know if the generated code is...

0693W00000QL2LCQA1.png

STM32CubeMX not working on Win11 for ARM in emulated mode

I've tried to run STM32CubeMX on my Windows 11 parallels virtual machine that run under Monterey on Apple M1 MAX machine.For some reasons the application crash. I've tried various compatibility modes with and without administrative rights but with no...

ABucs by Associate II
  • 1746 Views
  • 2 replies
  • 0 kudos