STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

STM32H7 SPI6 with BDMA

Hi,I have a project with an IOC configuring an STM32H733. In the IOC I configured the SPI6 in Full-Duplex Master. I also configured the BDMA channel 0 to serve requests of SPI6_TX. The project is pretty old and when I configured it like this I only e...

ANeam.1 by Associate III
  • 3971 Views
  • 4 replies
  • 0 kudos

Resolved! SWD Conflict w/ USART2 or System Wake-Up on STM32L0?

Using CubeMX to create a new project on the STM32L0X0 series. I need two UARTS, which this part offers. However, in CubeMX, when I try to enable the SWD, it creates a conflict is the SYS tab for "System Wake-Up 3". When I roll over this, it says it c...

jvavra by Associate III
  • 1890 Views
  • 1 replies
  • 0 kudos

Resolved! delay block problem octospi

I am using stm32l4r board to run some tests and i am generating my code with stm32cubemx, I am having an issue with the octospi parameters after investing with my colleagues and checking the documents we discovered it is a problem related to the dela...

JJuli.1 by Associate II
  • 3659 Views
  • 6 replies
  • 0 kudos

Interface SD card with nucleo H743ZI 1Bit/4Bit

How to interface SD card with STM32h743z1 nucleo borad ? Is there any working example? I generated code with cubeMx 5 and failed at the very first step.. I tried various threads regarding SD card and nothing helped me.card initialization itself giv...

In RM0401 Rev 3 and using the STM32F410, Table 62 page 373 shows that LPTIM can be used as a source trigger for TIM5 (slave). Is this possible?

I've noticed that there does not seem to be a trigger output selection for LPTIM. Is there a default operation I am missing?I've tried making LPTIM as the source trigger for TIM5 for the STM32F410 in the CubeMX IDE but can't seem to get it to work.I...

FArms.1 by Associate II
  • 1727 Views
  • 2 replies
  • 0 kudos

Resolved! Cube Bug on MCU SELECTOR ?

Hi, i need to find a mcu with 2 usb, min 512k of total ram and min 1024k of flash.When i put RAM and flash on selector, the result is mcu without USB, but you can see on list many mcu with 2 USB.The result is worst if you put on selector directly 2 u...

0693W00000Y99yJQAR.png
Marco1 by Associate II
  • 1621 Views
  • 2 replies
  • 0 kudos