STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Custom Makefile Template for STM32CubeMx

I have a couple of changes I would like to make to the Makefile generated by STM32CubeMx. My Toolchain/IDE is set to Makefile in the Project Manager tab. The default Makefile template has no places for custom user code, so every time the project is...

cvanbeek by Associate III
  • 920 Views
  • 0 replies
  • 0 kudos

Resolved! Problem of clock on STM32F107VCT6 on EasyMx Pro V7

Hello I'm using a STM32F1107VCT6 on an EasyMx Pro V7 dev board and I've a problem of clock. I create a project from STM32 Cube MX and I'm using STM32 Cube IDE for developing. I want to toggle a LED every 1 second. For this I'm using the library HAL a...

0693W00000Y96QnQAJ.png
Romano1 by Associate III
  • 2039 Views
  • 3 replies
  • 0 kudos

FMC_SRAM not work on STM32F7

Hello.I'm trying to use FMC Sram, but does not work.Here is what I tested.1) First, I downloaded FMC_SRAM example for Nucleo-H743ZI via STM32CubeMX. I want to see just NWE and NOE pin signal work when I call HAL_SRAM_R/W functions. And It worked as i...

0693W00000Y8iP7QAJ.png 0693W00000Y8iQoQAJ.png
DKOO by Associate
  • 1871 Views
  • 2 replies
  • 1 kudos

AN4776 questions?

These questions are wrt to synchronization section 2 AN4776 and CubeMX settings:When a timers input is selected as ITR0 and trigger/reset/gated mode is selected such that the timer is a slave....Is the clock of this timer it's own internal clock or d...

SWenn.1 by Senior III
  • 6318 Views
  • 1 replies
  • 0 kudos

I2C Custom Timing not available in SMBus mode (CubeMX)

Why CubeMX I2C Custom Timing MCU connectivity config option is unavailable in SMBus mode? Custom Timing is an advanced option for those which really know what they are doing and I do not think it makes sense to take it away in SMBus mode.On the oppos...

0693W00000Y740AQAR.png 0693W00000Y740FQAR.png
TDJ by Lead
  • 4219 Views
  • 8 replies
  • 0 kudos

Is it planned to generate CMake project?

Hi,are there plans on offering a generator for plain CMake projects?Currently the only way that works is to use CLion to convert the project to CMake but it would be nice if CubeMX supported CMake directly.

fsch by Associate III
  • 2923 Views
  • 6 replies
  • 1 kudos