cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX side by side install vs.firmware packages

Pavel A.
Super User

I've installed STM32CubeH7 library 1.10.0 manually from github.

I have CubeIDE 1.7 and CubeMX 6.3. Since they both do not understand STM32CubeH7 library version 1.10.0, I've installed CubeMX 6.5 side by side with v. 6.3.

The package manager of CubeMX 6.5 sees installed libraries v. 1.10.0 and v. 1.9.1. Fine.

But now both CubeIDE 1.7 and CubeMX 6.3 cease to see installed library v. 1.9.1, which they recognized before installation of CubeMX 6.5.

All CubeMX 6.5 and 6.3 and CubeIDE 1.7 see same installed versions of STM32CubeF0 and F4 libraries. What's the problem with H7 libraries?

OS: win11 home.

Update:

Ive removed subdirectory of v. 1.9.1. and reinstalled 1.9.0

Then all CubeMX 6.3, CubeMX 6.5, CubeIDE 1.7 see the package H7 1.9,0.

So it looks that patch H7 1.9.1 is too new for CubeMX 6.3/ CubeIDE 1.7

I don't understand why it was detected before install of CubeMX 6.5.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0