STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 2 kudos

UART2 Rx Interrupt Firing straight away

I have a problem using the NUCLEO-G431KB. After set-up of UART2_RX_INT, the interrupt seems to trigger and goes straight into the interrupt before any data has been put onto the receive pin of the UART. I have used Cube MX to generate the initalise. ...

PBens.3 by Associate
  • 2116 Views
  • 4 replies
  • 0 kudos

Timers not outputting PWM

I am using the Nucleo L476RG board and I have configured TIM2 to output PWM in Channel 1. I have very basic code that should output a 25% duty cycle because I set the PWM pulse in the TIM2 parameters settings to 250. I have tested several pwm pins an...

_legacyfs_online_stmicro_images_0693W00000bjJhgQAE.png _legacyfs_online_stmicro_images_0693W00000bjJhRQAU.png _legacyfs_online_stmicro_images_0693W00000bjJhqQAE.png
CDe S.2 by Associate
  • 2009 Views
  • 1 replies
  • 0 kudos

how to enter ADC1_IRQHandler

I have a stm32f030c8t6. I want to enable its ADC1 interrupt. in CubeMX, when I enable ADC DMA, there is no section where I can configure RANK. in the generated program, in stm32f0xx_it.c, I can see two functions belowvoid DMA1_Channel1_IRQHandler(voi...

Ala by Senior
  • 1913 Views
  • 1 replies
  • 0 kudos

There is a link to download STM32CubeIDE and STMCube32MX

Hi,I'm creating a Dockerfile and installing STM32CubeIde and STM32CubeMX with it. To install these two programs it would be very convenient to have a link to download the programs without human interaction.Is there a link to download them?Best Regard...

alex95 by Associate II
  • 1690 Views
  • 2 replies
  • 0 kudos

Can't open CubeMX project that was few minutes ago created

Created project with newest Cube MX, added all of my pin initializations, closed project, tried to open it - it does not open, no errors no warnings, shows that cubemx loads the file and then renders UI, always goes to 100% progress on both, and then...

TMark.14 by Associate III
  • 6569 Views
  • 13 replies
  • 0 kudos