Skip to main content
dmarks-ls
Associate III
Jul 15, 2025 9:05 PM UTC
Solved

STM32CubeMX 6.15.0 - Bug with STM32G0B1VE not having USB-C?

I pulled down the latest CubeMX (v6.15.0) to do a parametric search for a new part.  Needing > 70 GPIOs and USB device function but not much else, I narrowed in on the STM32G0B1 series.

When I start CubeMX, I'm told there are 4801 items in the parts list,  When I filter on "STM32G0B1", that drops to 103 items.  However... if I then filter on either "USB FS" or "USB Type-C", that number drops to 97 parts.  I exported a before and after and diffed the lists, and found that the 7 parts that fell out of the list were all STM32G0B1VE parts.  The 'VB (128K flash) and 'VC (256K flash) parts were in both lists, only the 'VE (512K flash) parts appeared to lack the "USB FS" and "USB Type-C" attributes.

This is a mistake, correct?  The 'VE parts have all the same peripheral features as the 'VB and 'VC parts, yes?

Dana M.

This topic has been closed for replies.
TDK
TDKBest answer
Jul 16, 2025 3:08 AM UTC

Yes, clearly a bug.

I've noticed the attributes here have a lot of inconsistencies in the MCU selector when looking for chips. This is surely not the only one.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
Jul 16, 2025 3:08 AM UTC

Yes, clearly a bug.

I've noticed the attributes here have a lot of inconsistencies in the MCU selector when looking for chips. This is surely not the only one.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Jul 16, 2025 5:04 AM UTC

Hello @dmarks-ls 

I escalated the request to involved people to fix this issue (Internal ticket number: 214160)

(Internal ticket number is only for reference, not accessible or usable outside of ST).

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Nov 20, 2025 2:29 PM UTC

Hello All,

I would inform you that this issue is fixed in the latest release of STM32CubeMX v6.16.0 published on st.com.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks