User Activity

Hello. I have a simple project, but I have a hard time doing my project in STM. The difficulty of the project is that all processes have to work at certain sampling times. As you can see in the picture, I have a robot that is controlled by 2 channel ...
Hello. I want to read multi-channel analog data (four channels) with my Nucleo-F072RB. I previously worked with Nucleo F411RE and I did not have any problems. But with F072RB, I'm so confused. When I open my board on CubeMX, I can select multi ADC1 c...
Hello. For a project, I need to read 4 channels analog data and save them in to the sd card for 10 seconds. I should record every data minimum with 750 Hz. And then I generate pwm signal with these data. I tried that but it was not successful, recor...
Hi. I have Nucleo-L412 programming error with Keil. I can program Nucleo F401, F411 and F407 discovery board without error. But I can not load the program to the L412 board. I had had "No ST Link Detected error" but then I solved this problem on Keil...