cancel
Showing results for 
Search instead for 
Did you mean: 

Bug on the "HAL_PWREx_EnableWakeUpPin" function on STM32H7

cb.7
Associate III

Hello,

I am using STM32H7B0VBT6 and I wanted to activate the wake up from Standby on PA0 (WAKEUP_PIN1) with rising edge, the code used is the following:

PWREx_WakeupPinTypeDef sPinParams = {0};

sPinParams.WakeUpPin = PWR_WAKEUP_PIN1;

sPinParams.PinPolarity = PWR_WAKEUP_PIN1_HIGH;

sPinParams.PinPull = PWR_PIN_NO_PULL;

HAL_PWREx_EnableWakeUpPin (& sPinParams);

However, I found that "PWR_WAKEUP_PIN1_HIGH" actually activates the falling edge and not the rising edge!

Instead, for example on WAKEUP_PIN4, the setting is done correctly.

Please fix in future releases of IDE libraries.

thank you!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0