STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1556 Views
  • 0 replies
  • 2 kudos

Resolved! CAN-Bus no callback/received frame; FDCAN STM32G473

I'm trying to attempt CAN on a STM32G473 MCU. While transmission seems to be fine, I'm not receiving any data back. The receive call back function is not triggering.Following is my setup:Below is the TxHeader and RxHeader initialization along with th...

_legacyfs_online_stmicro_images_0693W00000bjJuuQAE.png _legacyfs_online_stmicro_images_0693W00000bjJx0QAE.png
MMoha.10 by Associate III
  • 3019 Views
  • 2 replies
  • 0 kudos

Does Cube MX build the libc.a printf/canf/heap/etc library?

Yesterday's post herehttps://community.st.com/s/question/0D53W00002F4MHrSAN/is-there-a-bug-in-the-newlib-heap-on-the-32f417-cube-ide-library?t=1682872893044refers.This articlehttps://nadler.com/embedded/newlibAndFreeRTOS.htmlsuggests that the freerto...

PHolt.1 by Senior III
  • 6704 Views
  • 13 replies
  • 0 kudos

Can't install STMCUFinder on MacOS Ventura 13.3.

This is a prerequisite for the VSCode extension which is why I am asking here.Steps to reproduce:Download the setup filePer Readme.html, open a terminal, navigate to the en folder and run the following command: sudo xattr -cr ./SetupSTMCUFinder-5.0.0...

Resolved! STM32H755 Nucleo and PWR_DIRECT_SMPS_SUPPLY

Hi, I'm using an STM32H755ZIQ Nucleo and migrating an old project in CubeMX 6.8.The RCC > supply source > PWR_DIRECT_SMPS_SUPPLY option has been removed from CubeMX, which was the default previously. I tried the two available options (External / LDO...

MJack.1 by Associate III
  • 5815 Views
  • 6 replies
  • 1 kudos

Migrate from STM32H743 to STM32HA3

I have a project using a STM32H743 (LQFP144). I want to migrate it to a STM32HA3. It seems like it should be fairly pin compatible, but in Stm32CubeMX when I use the Alt-L (Pinout Compatible) option, the STM32HA3 isn't there. Is this a lag in the Cub...

DanF by Associate II
  • 2306 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeMx command line unknown pack STM32Cube_FW_G0_V1.6.0

Hi,I start STM32CubeMx with this command /mydir/STM32CubeMX/STM32CubeMX -q /mydir/myscriptInside the file myscript there are this lines:swmgr refreshswmgr install STM32Cube_FW_G0_V1.6.0 askexitWhen run this line "swmgr install STM32Cube_FW_G0_V1.6.0 ...

alex95 by Associate II
  • 1684 Views
  • 2 replies
  • 0 kudos