STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

Resolved! STM32G030K8T6 HSE Crystal Resonator Option Missing (CubeMX)?

Hello,I recently developed a board to use the STM32G030K8T6 under the assumption that it could support an external crystal oscillator (given what is said in the datasheet) and as I was setting it up in the CubeMX tool I noticed that the HSE was only ...

RGuin.3 by Associate
  • 3971 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeMX doesn't generate the project well, it left MXTmpFiles when I build the configurations.

Hello.I'm using the lastest version of STM32CubeIDE, 1.12.1.The problem occurs after configuring al the STM32CubeMX perifereals and I try to build the project so it generates al the files that I need. But when I press the yellow wheel icon, the proje...

_legacyfs_online_stmicro_images_0693W00000bj3aBQAQ.png

Wrong USART3 pins on Nucleo-F756ZG

Hi,On my Nucleo-F756ZG, when I generate code for USART3 that's by default connected to ST-LINK , Cube sets pins for morpho connector (PB10 PB11) instead of alternate function (PD8 PD9). I also use Nucleo-L476RG and for this board, Cube set alternate ...

Resolved! Generate Single pulse using timer using HAL / CubeMx

I have been reading reading anything i could find on Timers, but I'm still confused about the setup in CubeMx.I just want to trigger a timer in software, that generates a SINGLE pulse with a set width (and if possible after a set dely) on a pin, but ...

RKage.3 by Associate
  • 9216 Views
  • 6 replies
  • 10 kudos

Resolved! How to install STM32CubeMX on Ubuntu?

I ran "SetupSTM32CubeMX-6.8.0.sh", it was prompt:Check exe path on linux FullExe path1 is: /usr/bin/SetupSTM32CubeMX-6.8.0 Exe path is: /usr/bin Search java from relative path ---- Checking java in /usr/bin/./jre/bin/java Checking java in /usr/bin/.....

MQi.1 by Senior II
  • 11048 Views
  • 11 replies
  • 0 kudos

"Modified" column in GPIO configuration

Hello, what is meaning of the "Modified" column in GPIO configuration? When given pin is considered as modified? I am not able to find that information in CubeMX user manual...

_legacyfs_online_stmicro_images_0693W00000bjg2gQAA.png
MLaso by Associate II
  • 2360 Views
  • 2 replies
  • 0 kudos

NUCLEO-C031C6: Error when updating via MX

Good day,There seems to be an error in the implementation of the NUCLEO-C031C6 when generating code for the project after updating the peripherals. After loading an example project and compiling and testing all is well but once you update the project...

CKlib by Associate II
  • 4285 Views
  • 7 replies
  • 0 kudos