2022-08-15 4:18 AM
How do I get a callback function for the HAL_TIM_OnePulse_Start_IT function?
I have a STM32G071 Nucleo board.
I whish to start a one-shot timer that calls an interrupt callback function when the time has elapsed. For this I have chosen the timer 6 and had the CubeMX, to generate the code:
static void MX_TIM6_Init(void)
{
/* USER CODE BEGIN TIM6_Init 0 */
/* USER CODE END TIM6_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM6_Init 1 */
/* USER CODE END TIM6_Init 1 */
htim6.Instance = TIM6;
htim6.Init.Prescaler = 3;
htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
htim6.Init.Period = 40000;
htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OnePulse_Init(&htim6, TIM_OPMODE_SINGLE) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM6_Init 2 */
/* USER CODE END TIM6_Init 2 */
}I have then tried to start the timer with:
HAL_TIM_OnePulse_Start_IT(&htim6, TIM_CHANNEL_6);and then tried to get the ISR to toggle the LED with this code:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *TimHandle){
HAL_GPIO_TogglePin(LED4_GPIO_Port, LED4_Pin);
}And this code:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *TimHandle){
HAL_GPIO_TogglePin(LED4_GPIO_Port, LED4_Pin);
}But none of these are working.
What am I doing wrong?
Solved! Go to Solution.
2022-08-16 1:44 AM
Thanks for your suggestions Jaroslav
I actually found a solution to the problem, by watching this video; that has a an example that uses OnePulse:
https://www.youtube.com/watch?v=3yvY7pLMHAg&t=289s
And what I found that were missing in order to make my code work was this as a part of the timer init:
/* USER CODE BEGIN TIM6_Init 2 */
// Clear interrupt bit in SR that was set as a side effect of generating an update event in TIM_Base_SetConfig
__HAL_TIM_CLEAR_IT(&htim6, TIM_IT_UPDATE);
// enable timer update interrupt
__HAL_TIM_ENABLE_IT(&htim6,TIM_IT_UPDATE);
/* USER CODE END TIM6_Init 2 */The timer pulse-width were set with:
htim6.Instance->ARR=20;I could NOT make the code work, with start of timer by:
HAL_TIM_Base_Start_IT(&htim6);
HAL_TIM_OnePulse_Start_IT(&htim6, TIM_CHANNEL_6);so I started the timer with:
__HAL_TIM_ENABLE(&htim6);like described in the video.
The interrupt handler were:
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
if(htim==&htim6) // check source
{
transmissionReceived=1;
}
}
/* USER CODE END 4 */(Like you also suggested :smiling_face_with_smiling_eyes: )
2022-08-16 12:40 AM
Hello,
you have to start the timer with:
HAL_TIM_Base_Start_IT(&htim6);
HAL_TIM_OnePulse_Start_IT(&htim6, TIM_CHANNEL_6);In your case, the UIE bit in DIER register is not set and the interrupt is not enabled.
The IRQ handler will then call your HAL_TIM_PeriodElapsedCallback() function and toggle the pin.
-- Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-16 1:44 AM
Thanks for your suggestions Jaroslav
I actually found a solution to the problem, by watching this video; that has a an example that uses OnePulse:
https://www.youtube.com/watch?v=3yvY7pLMHAg&t=289s
And what I found that were missing in order to make my code work was this as a part of the timer init:
/* USER CODE BEGIN TIM6_Init 2 */
// Clear interrupt bit in SR that was set as a side effect of generating an update event in TIM_Base_SetConfig
__HAL_TIM_CLEAR_IT(&htim6, TIM_IT_UPDATE);
// enable timer update interrupt
__HAL_TIM_ENABLE_IT(&htim6,TIM_IT_UPDATE);
/* USER CODE END TIM6_Init 2 */The timer pulse-width were set with:
htim6.Instance->ARR=20;I could NOT make the code work, with start of timer by:
HAL_TIM_Base_Start_IT(&htim6);
HAL_TIM_OnePulse_Start_IT(&htim6, TIM_CHANNEL_6);so I started the timer with:
__HAL_TIM_ENABLE(&htim6);like described in the video.
The interrupt handler were:
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
if(htim==&htim6) // check source
{
transmissionReceived=1;
}
}
/* USER CODE END 4 */(Like you also suggested :smiling_face_with_smiling_eyes: )