cancel
Showing results for 
Search instead for 
Did you mean: 

NO ADC DMA interrupt on F446RET6, CubeMX 6.7.0, FW4_1.27.1

sfrwmaker
Associate II

Hello!

I have faced the problem with ADC checking using DMA on my F446RET6 MCU. The software tools are CubeMX 6.7.0 and CubeIDE 1.10.1. The Firmware is FW4_1.27.1. Perhaps, it is my mistake, but i canntot understand how to fix it. Here is the simple project directory in cubeIDE https://www.dropbox.com/s/g1o8yunmubjjmk1/F446_ADC_DMA.zip?dl=0 together with .ioc file.

After HAL_ADC_Start_DMA(&hadc3, (uint32_t*)c_buff, ADC_CCONV); call there is no HAL_ADC_ConvCpltCallback() interrupt, yet i could not capture the interrupt inside the standard DMA2_Stream0_IRQHandler().

Looking forward for your advice.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @sfrwmaker​,

Could you disable your WWDG Mode, it works just fine for me.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

1 REPLY 1
FBL
ST Employee

Hello @sfrwmaker​,

Could you disable your WWDG Mode, it works just fine for me.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL