2022-12-20 1:58 AM
I have wrote an product with tcp communication, last modification September 2021...
Today I need a small evolution ( move from HSI-RC to HSE)...the Ethernet does not run now.
I have try to work with doc concerning the new driver versus legacy...
help-me.
Eric
2022-12-20 2:51 AM
Does it work with the new driver before changing the clock source from HSI to HSE?
2022-12-20 3:00 AM
All the application is running (FreeRTos, CAN, USARTs, timer, GPIO) but it does not send TCP packet.
I try to DO NOT change my code... just config 8742 in CubeMx...
I use tcp_send, tcp_write,tcp_sndbuf, tcp_output, tcp_abort, tcp_close......
2022-12-20 3:06 AM
Today I work back on the old hardware with HSI-rc to try to minimize the problemssss
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.