STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 2 kudos

Resolved! Help with MX

I'm a new user to STM32CubeMX. I tried to generate code for IWDG on the STM32F746NGHx and the pProject Manager Setting dialog appeared saying 'The Firmware Package (STM32CU FW_F7V1.17.1) or one of its dependencies required by the Project is not avail...

scotte by Associate
  • 3133 Views
  • 4 replies
  • 3 kudos

Custom packs path in IOC files

I've been using CubeMX for the last 2.5 years and am in the process of updating our ioc files to the latest version of the CubeMX software, the latest STM32 Firmware and to use AzureRTOS rather than the old ThreadX and NetX releases from Express Logi...

SPI interface characteristics

Hi. I am selecting for chip upgrade. In the database content of STM32H743ZG, the SPI interface characteristics section says that the VOS level should be set to VOS1 as shown in the picture, but I chose rev.V to use the main frequency 480 MHz. So my V...

giwonKIM_0-1716441403001.png
giwonKIM by Associate III
  • 1419 Views
  • 1 replies
  • 0 kudos

Resolved! How to install a patch offline in the STM32Cube IDE?

in https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-mcu-mpu-packages/stm32cubef4.html there are the MCU package and the patch, the first can be installed from CUBE IDE with "m...

Resolved! STM32H573 UART9 initialization not working

use STM32CubeMX to get the initialization code,but UART9 not work,use the LL LibraryUART9 initializationvoid MX_UART9_Init(void) { LL_USART_InitTypeDef USART_InitStruct = {0}; LL_GPIO_InitTypeDef GPIO_InitStruct = {0}; LL_RCC_SetUARTCloc...

xkl by Associate II
  • 2107 Views
  • 4 replies
  • 0 kudos

STM32CubeMX always enables UART5 interrupt

Hi All! Using STM32CubeMx 6.11.1, and the STM 32L475 processor, I have successfully configured UART 5 to use DMA with interrupts on TX and just interrupts (no DMA) on receive. But whatever I do, STM32Cube seems to generate these lines: /* UART5 inter...

Vandermyer_0-1716368071597.png

LevelX Setup for MX25R6435 on B-L4S5I-IOT01A

Attempting to create a project to access the onboard QuadSPI NOR flash (MX25R6435) on the SM32L4S5 Discovery kit. In STM32CubeMX, select the MX25R6435 under QuadSPI HAL says there is no QuadSPI HAL flash driver available, even though the stm32l4xx_ha...

SLimi.1 by Associate III
  • 2134 Views
  • 1 replies
  • 0 kudos

ST generated code warning

Hello,Getting a lot of these warnings in the ST generated code - prefer to be warning free, so legitimate, application code warnings are more obvious. I don't see the ability to suppress individual occurrences, and don't want to remove -Wregister com...

R_DSP_0-1716244187560.png
R_DSP by Associate II
  • 2165 Views
  • 3 replies
  • 1 kudos

Generate peripheral initialization to specific directory

STM32CubeIDE 1.10.1STM32CubeMX 6.6.1-RC2 In CubeMX -> Project Manager -> Code Generation there is an option to generate separate file pairs for the peripherals. These files are generated in the Core\Inc and Core\Src folder. Is there a way to have the...

gb2835 by Associate II
  • 1420 Views
  • 1 replies
  • 1 kudos