STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1586 Views
  • 0 replies
  • 2 kudos

Resolved! DCT Issue: Missing HAL Interrupt Handler for USART6

Hi everyone,I'm encountering an issue with the STM32 Device Configuration Tool: it doesn't properly generate the global interrupt handler function for one of the UARTs in my project: The generated interrupt handlers for USART1 and USART2 include call...

How to install x-cube-eeprom on STM32Cube?

Hello, I have downloaded en.x-cube-eeprom_v4.0.0.zip but I do not know how to install it on STM32Cube. It should have been a package installed "from local" and selected the zip in STM32Cube MX? Or what I need to do is copy all the files for my projec...

FCOST.1 by Associate II
  • 12838 Views
  • 11 replies
  • 7 kudos

Installing CubeMX 6.13 -console Error

I have tried to install the latest CubeMX software 6.13 in silent mode. Unfortunately the installation fails with the following error code in debug mode: 'ProcessBuilder.start(): pid: 95163, dir: null, cmd: “net”'I have executed the installation with...

Crankzz by Associate
  • 1785 Views
  • 3 replies
  • 0 kudos

USB HS - USB_TIMEOUT in stm32h7r3z8t6

Hello,I am working on a custom board with stm32h7r3z8t6. After the definition of the USB HS in Cube MX, the USB initialization is stuck on USB_TIMEOUT: USB HS connection on the board:  Here is the clock config:  void SystemClock_Config(void){RCC_OscI...

MihavinVin_2-1736260768989.png MihavinVin_3-1736260959083.png MihavinVin_4-1736261000481.png MihavinVin_0-1736260554509.png

Can't seem to start SPI1 on Nucleo-F401RE

I've been struggling for a while now to start the SPI1 protocol on the Nucleo-401RE. According to the datasheet, SPI1 is connected as follows, I generated the code in CubeMX and without adding a single line of code, compiled it without any failures a...

0690X00000ARHqoQAH.png
malehakim by Associate III
  • 2861 Views
  • 4 replies
  • 0 kudos

Resolved! Problems with CAN on STM32H753 after migration to CubeMX 6.13

Hi everyone!I've migrated my STM32H753 project to the new CubeMX version, and after that, something went wrong with the CAN bus communication (everything worked fine before the update). The CAN functions return no errors, and messages are being sent,...

tuo by Associate II
  • 3155 Views
  • 9 replies
  • 1 kudos

TIM8 STM32H745 PWM mode 1

I am using the STM32H745i_DISCO board. I can't seem to get TIM8 to output on PK0. I sure the GPIO is be setup correctly, but there must be something in one of the TIM8 registers. I am attempting to use TIM8 to adjust the brightness on the LCD screen,...

eadboston_0-1736199838299.png eadboston_1-1736199886380.png eadboston_2-1736200071656.png

Resolved! Modifying USB descriptor values in CubeMX

Hi,I am working on USB Device Middleware on STM32F469NI using STM32CubeMX. For our use case we have to modify the PRODUCT_STRING descriptor value (default is "STM32 Virtual ComPort"). Is it recommended to perform this, or are there any STM standards ...

nagahimanshu7_0-1736169522474.png