STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX crash

Hello STM,My STM32CubeMX crashes randomly. I've attached the ioc file so you can run some tests and see for yourself. I tried to make some changes to my original project, and as I reopened the ioc it came up with this message: After that, I created a...

Intector_0-1738378509380.png Intector_1-1738378674728.png Intector_2-1738379016368.png Intector_3-1738379089387.png

STM32WL: RTC stops LoRa from working

Hello guys, I'm currently working on a project with the STM32WL board, and using the LoRa application.I'm having a problem with the RTC, what happens is that for the project I'm using the PingPong LoRa example, and I don't know exactly what is the in...

FPicc.1 by Senior
  • 3520 Views
  • 5 replies
  • 0 kudos

TIM Trigger DMA

I want to use two timers: one timer to generate PWM, and another timer to generate periodic interrupt events to trigger DMA. For example, use TIM2 to output PWM, and TIM3 to periodically generate update events to trigger DMA for updating the duty cyc...

smile by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos

Resolved! How create STM32CubeCLT CPP Project with VS code

Hi all,I transfer development from STM32CubeIDE to VS code with STM32CubeCLT and STM32CubeMX.By default, the CMake project generated by CubeMX uses C language, but my target language, which includes C++ modules, is supported. I wonder how to add a cp...

Nhan by Associate II
  • 2192 Views
  • 2 replies
  • 1 kudos

Neural Network Deployment

I want to deploy my model in STM32 F446RE for validation on target, I will connect my STM32 via a mini USB cable to the laptop.Now guide me in details for each step (such as pinout & configuration, connectivity and others)Please help me

STM32F756 Ethernet and lwIP Rx and Tx Descriptor

Hello,I am creating a new project using STM32CubeIDE to use lwIP with internal MAC for a Nucleo F756 Board. When I enable the Eth peripheral, I can configure the Rx and Tx descriptors. They are placed at the start of SRAM2 (0x2004C000).Since the Cube...

descriptors.png descriptors.png new_region_sram2.png new_region_sram2.png

HAL RTC SetDate Bug or some another way to do??

Posted on February 23, 2017 at 10:49I am using STM32F103 in my new application. I have used STM32Cube to generate my code including Internal RTC. Myproblem is that the time is ok saved when reseted but date is always reset. when i inspected the code...