STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 2 kudos

Resolved! SMPS on the STM32H747XI

I have created a project for the STM32H747I-DISCO and have deadlocked the MCU twice. a BIG thanks to ST for not having ANY warning about this. The DISCO board comes configured to default to SMPS mode. The project I created, without any warnings, defa...

Hal56-GCI by Associate III
  • 1995 Views
  • 4 replies
  • 2 kudos

NUCLEO-C071RB Interrupt problem

I tried this board but i get some problem about interrupt.I "writed" only 1 function ( void EXTI0_1_IRQHandler(void) ) the other code has been autmaticaley generate from Cube.The goal is : for any change of state of PA0, pulse_count++.The problem is ...

Resolved! How to map OCTOSPIM to port G on STM32U5Axxx

I'm new to STM32CubeMX and have difficulties finding out how to map all OCTOSPIM_P2 signals to Port G. I can manually map some signals to Port G (CS, IO[7:4], DQS), but can't figure out how to map the rest.  Any help most welcome!

MikeStrom by Associate II
  • 1959 Views
  • 4 replies
  • 2 kudos

STM32CubeMX v6.13 cannot open .ioc file for H56

I recently updated my version of CubeMX from 6.12.1 to 6.13.0. It is now unable to open my .ioc for a specific STM32H563VI project. When I try to migrate, it loads the IOC, then gives an error saying it is "Not a valid ioc file".If I try to continue ...

EskayEllar_0-1734042731864.png

Resolved! TIM6 & DAC question on STM32F469I-DISCO board

Using STM32 CubeMX ver 6.9.2, if you start a new project using STM32F469I-DISCO board and choose Yes to set all peripherals to their default settings, TIM6 comes up disabled/gray. Why is that? Instead of pinout view, choosing system view, only shows ...

Resolved! CMake project generation with CubeMX + CubeAI fail

Hello,I use STM32CubeMX V6.11.1 with cmake version 3.28.1 (the one embedded in STM32CubeCLT_1.15.1) to generate a project for STM32F746G Discovery kit.When trying the new cmake project generation feature in conjunction with CubeAI, the generated proj...

jjaccard by Associate II
  • 4172 Views
  • 6 replies
  • 1 kudos