STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 2 kudos

Output Compare Register update in stm32

I had taken TIM1 asn Master to Trigger TIM8 here below i had attached the timer configuration Clock Frequency 480mhz ,timer clock 240mhzHere Iam Triggering The TIM8 after 2.5us started from TIM1 both are 100khz frequency in TIM->CCR3 register iam loa...

IMG20250205175541.jpg IMG20250205175611.jpg IMG20250205175558.jpg

STM32CubeMX: TSC Advice

Well I got the new board back it seems to work, but it's quite different: I have 3 groups of 3 sensors and one group used for the shield. Previously Cube MX defined this as 3 Banks, now it has defined 6 Banks. Should I worry about this? In the first ...

Lanceh by Associate III
  • 1291 Views
  • 3 replies
  • 0 kudos

Difference in Generated Files: STM32Cube.AI GUI vs. CLI

When generating code using STM32Cube.AI GUI, I get all the necessary project files.However, when using the CLI, I only get the model's .c and .h files. Is there a command to generate all the additional files via CLI? Or can anyone explain the differe...

mkothuri by Associate II
  • 1011 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 5.5 does not generate CMSIS DSP files

I've created a STM32CubeMX project for stm32f411re uC and try to add CMSIS DSP suppor. I go to "Aditional Software" -> ARM.CMSIS and check CORE 5.3.0 and DSP 1.7.0. Into DSP I chose Source. CubeMX download the CMSIS package into STM32Cube/Repository/...

leonardo by Associate III
  • 10718 Views
  • 17 replies
  • 4 kudos

Resolved! Cannot Analyze Keras Model

Hi STM community, I'm a fairly new user of the STMcubeMX software. I followed this tutorial (https://youtu.be/grgNXdkmzzQ?si=gDybMlGQxgTNwpPC) and every time I try to analyse my model under the 'MCU/MPU Filters' tab it just stays greyed out and does ...

ramyg1_0-1738520699368.png
ramyg1 by Associate
  • 1121 Views
  • 1 replies
  • 1 kudos