STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Core cm3

Posted on June 21, 2011 at 10:18extern uint32_t __get_PSP(void); Hello, When I compile an example, I have all these errors, they said incomptabile declaration for all the folowing list: extern void __set_PSP(uint32_t topOfProcStack); extern uint32_t...

cyril2399 by Associate II
  • 1377 Views
  • 2 replies
  • 0 kudos

STM32F100R4H6 SMBus interrupt problem

Posted on July 01, 2011 at 15:21HI..in attach file there's my code. i've to manage smbus using interrupt (no polling allowed). I don't understand why the interrupt doesn't start. The code doesn't me any error. Is it correct manage the smbus protocol...

Calling RTC_Init

Posted on June 27, 2011 at 12:13Good morning everybody! I'm evaluating ST standard device Library with STM32L discovery board. I want to test RTC and so in my main I want to call RTC_Init and so on. So I prepare a RTC_InitType  structure, I create a...

Interupt priorities

Posted on June 28, 2011 at 09:38Hi All, Can anyone explain the difference between the prem and sub interupt priorities.  For example what TIMER_1_IRQ_PREM_PRI and TIMER_1_IRQ_SUB_PRI. -- Thanks #stm32-c-embedded

RTC calendar on STM32F100x

Posted on June 29, 2011 at 13:02Hi, i've to implement a RTC calendar on my STM32F100 microcontroller. I've the RTC library, but i'm searching a so called ''calendar.h'' that already has defined: days, weeks, months,years etc.. Some ideas?? #time...

Any good (In depth) STM32 I/O tutorials?

Posted on June 26, 2011 at 19:08I've built a gas turbine engine, which currently runs on a variety of manual valves/switches to run. What i want to do is to install solenoids into my fuel rings/pump supply, and relays on the switches controlling my ...

Hard Fault Error - STM32F100C8

Posted on June 27, 2011 at 12:34I am trying to implement EEPROM emulation in the flash memory. I am able to write and read the data from flash. When trying to write the second data it is going to HARDFAULT Error. I m not sure why this happens. Belo...

ezyreach by Associate II
  • 4784 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.