Question
RTC prescaler load register is always to default on RESET?
Posted on June 24, 2011 at 16:49
Hello,
I have: a STM32F103RC, a fresh 3V Li BATT, a 32.768kHz crystal and my own RTC support library. I works, but... The manual RM0008 (Doc ID 13902 Rev 11), page 454, says:If the input clock frequency (fRTCCLK) is 32.768 kHz, write 7FFFh in this register to get a signal period of 1 second.So I do this but I noticed, the RTC_PRL register became 8000h (its default reset value) every time I started debugging as if it were not in the back up domain! Any ideas? TIA.