STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Device Library Bug (STM32F2XX, STM32F1XX)

Posted on March 25, 2012 at 14:30Found a bug in the USB Host / Device library.uint32_t overflow, max. block number is ~ 8.4M.See the link, rows 39 - 40https://gist.github.com/f4691b584575c41e26fbIs there any chance to have this bug (and others too) ...

dzuikov by Associate II
  • 955 Views
  • 1 replies
  • 0 kudos

TIM2_CH1_ETR as an external event to clear OCxREF.

Posted on March 26, 2012 at 05:23Hi,     I'm trying to operate the TIM2_CH1_ETR as an external event to clear OCxREF. I have configured:1) PA0 as TIM2_CH1_ETR Alternate function and2) PB11 as TIM2_CH4 PWM output.I'm trying to implement what is descr...

mary11 by Associate
  • 717 Views
  • 0 replies
  • 0 kudos

TIM2_CH1_ETR as an external event to clear OCxREF.

Posted on March 26, 2012 at 05:19Hi,     I'm trying to operate the TIM2_CH1_ETR as an external event to clear OCxREF. I have configured:1) PA0 as TIM2_CH1_ETR Alternate function and2) PB11 as TIM2_CH4 PWM output.I'm trying to implement what is descr...

mary11 by Associate
  • 690 Views
  • 0 replies
  • 0 kudos

Using USB OTG as a device

Posted on February 25, 2012 at 19:23I need to use a F105 as I need CAN and USB at the same time. I need to connect it up with a B type connector as a device only. The manual talks about device and peripheral, but I always thought they were the same ...

DiBosco by Senior II
  • 1819 Views
  • 5 replies
  • 0 kudos

STM32 AN2581 Application Note and Source code

Posted on March 24, 2012 at 20:24In the web by google I have finded the ST AN2581 Application note with same example to configure the TIM Peripheral. The application note says that for any example there is a source code on the site http://www.st.com...

High power consumption in StandBy mode

Posted on March 21, 2012 at 16:53 Hi I have my F205 (and F405) going to StandBy mode and waking up properly. I have confirmed that from the PWR_CSR register's SBF flag and also the 25MHz HSE is turned off properly according to an oscillo...

tuomas by Associate II
  • 2100 Views
  • 5 replies
  • 0 kudos

Troubles setting up the CAN

Posted on March 24, 2012 at 11:39Hi, I'm having troubles setting up the CAN bus on my STM32F103R4. I'm using the can example from the keil homepage . When it is about to leave initialization mode, hardware doesnt reset the INAK bit in MSR register ...

STM32F2xx FSMC interfacing with SDRAM memory

Posted on March 22, 2012 at 17:13Hi,First of all i know that FSMC in STM32F2xx does not support SDRAM devices. But i think that with little effort it should somehow work reasonably.A good example of how the others try to this is at http://www.myplac...

STM32F100C8 seems to have 128k flash despite datasheet

Posted on March 23, 2012 at 16:34we made EEprom emulation tests with the discovery board first (with 128k of flash). Our own target uses the C8 processor. We have not paid attention to flash size in regard with eeprom, but did not run into problems,...