STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Warning: limit simultaneous DMAs to 2

Posted on January 14, 2012 at 01:53We've been working on this problem with the F2x and F4x for some time, and figure it's about time to warn others about what we've found. You can find the full details here:http://blog.frankvh.com/2012/01/13/stm32f2...

Remapping USART3 to SPI3 @STM32F107 not possible?

Posted on August 22, 2012 at 20:57Hello everyone,I am working with the STM32F107 chip on the STM32F107VC board from IAR.The evaualtion board has an LCD which has as its inputs SPI3_MOSI and SPI3_SKC. But since it needs to have 9 bit inputs, i can co...

dbeken by Associate II
  • 2095 Views
  • 6 replies
  • 0 kudos

Interfacing OV5620 sensor with stm32f103

Posted on August 10, 2012 at 13:43Hello,i have interfaced ov5620 sensor with stm32 vl discovery board.....it is a 5 MP camera sensor....the problem is i am getting multiple frames in my image...i am getting this image through video port.....can any ...

pawan by Associate
  • 1359 Views
  • 1 replies
  • 0 kudos

SPI change polarity on the fly

Posted on August 22, 2012 at 18:30Hi, I want change polarity on the fly example When I setting the SPI master, I setting ''SPI_CPOL_Low'' trasmit the 16 bit data, and work! But I need recive another 16bit data with polarity inverse ''SPI_CPOL_Hight'...

0690X00000602lmQAA.jpg

STM32F103 / Olimex H103 and debug Printf in Keil

Posted on August 22, 2012 at 14:17Hello everyone. I am currently on a project involving STM32F103, and for this I have the following hardware : - STM32-H103 Olimex board - Ulink2 interface - Keil uVison 4.54. I have been trying recently to setup pro...

0690X00000602lhQAA.jpg 0690X00000602fqQAA.jpg 0690X00000602dyQAA.jpg
longchair by Associate III
  • 887 Views
  • 0 replies
  • 0 kudos

Problems with FPU STM32F4

Posted on August 21, 2012 at 12:13Dear STM32 experts,i want to use the FPU of my STM32F4Discovery. So i did the following compiler options:-Arm Architecture: v7EM-Arm Core Type: Cortex-M4-Arm FPU Type: FPv4-SP-D16-GCC Target: arm-unknown-eabiAfter t...

Errors in firmware ?

Posted on August 21, 2012 at 11:33Hi. As i m currently working on an application running on both STM8S and STM32, i'm using firmware libraries to get a portable code. i already found several mistakes. As an example : Software NSS bit. - first mistak...

thibaut2 by Associate II
  • 2649 Views
  • 5 replies
  • 0 kudos

STM32F0 Timer16

Posted on August 21, 2012 at 19:34Hi, I have a problem with Timer16 of STM32F0 Discovery. I want use this timer like ''time base'' one interrupt at 1mS. It Works but this timer has a ColockDivision ? Because when I setting the ColockDivision  at :1 ...