STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

need a working code for CAN protocol by stm32f3 discovery kit

Posted on May 07, 2013 at 14:01hello ,i check STM32F3-Discovery_FW_V1.1.0 folder where all example for stm32f3 discovery is given . but here is no project for CAN protocol . please send me code example or link from where i can get the working code ....

raj2 by Associate II
  • 1089 Views
  • 2 replies
  • 0 kudos

AN3990 firmware

Posted on May 03, 2013 at 18:25Hi guys,I cannot find source code for AN3990; there is someone that can kindly give me the right link? Thank youMarco #an3990

STM32F400 and CS42L52 audio codec

Posted on April 16, 2013 at 13:09Hi! I have a big problem and need a lot of help. First of all I will try to explain the global situation and after that I will ask you for some questions. I am working in a project. I have to make a full-duplex audio...

rafael23 by Associate II
  • 5977 Views
  • 15 replies
  • 0 kudos

RS485 modbus Communication

Posted on March 25, 2013 at 13:01i am using the stm32f107rc  controller for rs485 communication. i am trying to transmit a set of data through usart1 from the controller, but some byte of data are missing at the destination so pls let known where i ...

aru by Associate II
  • 3689 Views
  • 5 replies
  • 0 kudos

eclipse+gcc+openocd+FreeRTOS

Posted on April 18, 2013 at 13:38Hello, Am using eclipse+gcc+openocd+FreeRTOS to setup an open Development Environment  for complex STM32 based embedded application.  I'm very new to building with GCC in general and I have never used FreeRTOS, but I...

Common Ext IT 15_9, Two Interrupts allways occur

Posted on April 30, 2013 at 08:37Hi together, I�ve got a problem which I just can not fix... I can�t figure out what is wrong. It would be very kind to help me out. It�s all about Interrupts. I want to use 3 external Interrupts comming from the Hard...

a_ by Associate II
  • 2550 Views
  • 4 replies
  • 0 kudos

STM32F105 CAN bus baud rate

Posted on May 05, 2013 at 10:24Hi, I am currently working on a project that require to monitor the CAN bus for specific data and once it received the data it will process and store on to flash memory. The data come in high volume bursts. One of the...

Measuring a sinewave

Posted on May 03, 2013 at 11:19Hello everyone, I am trying to measure a sinusoid signal via ADC. I used timer's trigger to obtain different samples. But i don't know how i can synchronize the trigger's time with the frecuency of the signal, to obtai...

montoya by Associate
  • 898 Views
  • 2 replies
  • 0 kudos