STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 - I2S sending & receiving

Posted on May 23, 2013 at 12:06 Hi togehter, I've some questions about the I2S interface of the STM32F405 microcontroller. I hope someone could help me I'm in a bit of a crisis here now. First to my hardware setup: I've the micr...

manuel by Associate II
  • 1816 Views
  • 1 replies
  • 0 kudos

SDADC full scale

Posted on May 17, 2013 at 10:09HiWe are using STM32F373 for the first time in our units and a problem with SDADC full scale occurred. We use it in a simple resistor measurement circuit:Circuit compares Rx with a know Rref resistor. Controller is sup...

0690X00000602obQAA.jpg
bpacan by Associate II
  • 2236 Views
  • 6 replies
  • 0 kudos

MCU running too slow?

Posted on May 20, 2013 at 08:44 So I've been noticing recently that my stm32f4 discovery board is running under 168 MHz. Or at least I think. I'm trying to get this loop uint32_t i = 0; for (;i<76799;i++) { GPIOD->ODR = 0x4100; GPIOD->ODR...

stm32f207 code protection

Posted on May 05, 2013 at 00:45Hi again.I have made great strides in our system this past week (our first use of the stm32) and we have had great interest in this latest (stm32 based) product from potential customers and therefore we would like to s...

adrian by Associate III
  • 1660 Views
  • 2 replies
  • 0 kudos

Timer overflow when in PWM mode?

Posted on May 20, 2013 at 09:18Hello,I'm running my code on STM32F103 chip, I've set up a PWM output from timer1 with period of 200 ms, pulse width 5 ms, it's working and can be seen with a scope on GPIOA_8. The thing is, that I want to do something...

Syncing USART/DMA RX

Posted on May 20, 2013 at 22:38I am using a STM32F407 and have set it up for using USART with DMA. I have some problems with the RX part. What is the best way to sync the enabling of the RX DMA with the remote transmitter? If I enable it in the midd...

NVIC and invalid SCB->ICSR register with DMA2

Posted on March 14, 2013 at 20:55Environment is an STM32F205VF on a custom board, but the problem has also appeared on a STM3240G eval board with an STM32F407I.  Compiler is GCC 4.6.2 at optimize level O0 for debugging. My application has extensive ...

f4-discovery, fpu not working in timer interrupt?

Posted on May 21, 2013 at 16:55Hi, I'm testing the f4 and the fpu. I have a small fpu test like this:volatile float a=0;volatile float b=.1;int c;for(;;)    {      GPIOD->ODR^=0x8000;      for (c=0;c<100;c++)        a=a+b;    }So by looking at PD15 ...

ian239955 by Associate II
  • 1457 Views
  • 3 replies
  • 0 kudos

HardFault_Handler exception...

Posted on May 16, 2013 at 13:53Hello,I'm using the STM32F4 on the discovery evaluation board.I wrote a simple function that calculates the mean of a vector. When the code is starting to make the summation it goes to HardFault_Handler...Here is the m...

0690X00000604sxQAA.png
yoav by Associate II
  • 4442 Views
  • 10 replies
  • 0 kudos

STM32F2xx OTP issue

Posted on April 02, 2013 at 16:47I need to put some data permanent in the OTP. But I phase a few problem durring debbug. 1. When try to program it on power up like in the FLASH I get the error can't program address 0x1FFF7800 as it is not a part of ...

Barbie by Associate II
  • 4385 Views
  • 14 replies
  • 0 kudos