STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STemWin Library

Posted on September 23, 2013 at 16:07I need to download STemWin Library,can you help me?thanks :)

aymen by Associate II
  • 1037 Views
  • 2 replies
  • 0 kudos

Problem with ADCs in dual regular mode

Posted on September 23, 2013 at 08:42I�ve have a problem with the ADCs in dual regular simultaneous mode. I want to measure 3 channels with ADC1 and 3 channels with ADC2. The conversions are started by software. I want to get 32 acquisitions in DMA ...

STM32F0 TIM15 ADC DMA, no DMA transfer

Posted on September 23, 2013 at 14:34 Hello! I want to get defined number of samples at constant sample rate. I used ADC1 triggered by TIM15 TRGO signal and DMA in normal (not circular) mode with interrupt on transfer complete. Something is wro...

mike2001 by Associate II
  • 1083 Views
  • 1 replies
  • 0 kudos

STM32F3 Timer3 and Timer4 as PWM

Posted on September 22, 2013 at 22:46Hi,  i use a STM32f3discovery evaluation board and trying to generate 6 PWM signals. For this purpose i have choosen Timers 3 and 4. As base project i use a Demo project. (The project demonstrates a sensors func...

dmytro by Associate
  • 2391 Views
  • 4 replies
  • 0 kudos

Timer to generate SPI clock

Posted on September 22, 2013 at 20:50I am currently reading a high speed ADC over SPI1.  E11 is configured to generate a DMA SPI write/read when the busy signal from the ADC goes low.  A double buffered DMA moves the data from SPI to memory.  Works ...

holcomb by Associate
  • 759 Views
  • 0 replies
  • 0 kudos

F103 not generating spi tx buffer empty interrupt?

Posted on September 20, 2013 at 18:13 I am puzzled over a missing SPI TX buffer empty interrupt at the end of a transmission. In slave mode I transmit x bytes and disable the tx interrupt when a new tx empty interrupt is generated after the ...

bernd by Associate II
  • 1686 Views
  • 2 replies
  • 0 kudos

support for stemwin on stm32f4 discovery

Posted on September 11, 2013 at 08:51Dear sir,            I'm using stm32f4discovery board with DM-STF4BB Base Board and DM-LCD35RT 3.5 inch LCD with touch screen. You can look for details in http://www.embedinfo.com/. Now I need to use your STemWin...

sen by Associate II
  • 1742 Views
  • 4 replies
  • 0 kudos

STM32F4Discovery + STemWIN

Posted on September 16, 2013 at 14:58 Hy guys, I have a problem whit Stm32F4Discovery with 3,5LCD (SSD2119 LCD driver) and STemWIN port. I download the examples from the st website, and try to port to discovery but not working. I have a ...

totti001 by Associate II
  • 1330 Views
  • 4 replies
  • 0 kudos