STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EXTI4_15_IRQHandler

Posted on July 01, 2014 at 09:01 Hi, I'm developing with STM32F0 and I have a problem with interrupt. this is my code: void batchStandByConf(void){ EXTI_InitTypeDef EXTI_InitStructure; //PC10 input GPIOC->OSPEEDR |= GPIO_OSPEEDER_OSPEE...

mosine by Associate II
  • 1310 Views
  • 0 replies
  • 0 kudos

Is STM32Lxxx compatible with STM32Fxxx?

Posted on June 27, 2014 at 14:43Hi; I recently noticed the STM32L family, while I already took a closer look at (and worked with) the STM32F family. At first glance it seemed to me that the STM32L05xxx are pin compatible with the STM32L05xxx. So her...

mmensch by Associate II
  • 1672 Views
  • 5 replies
  • 0 kudos

STM32 in DIP and SO packages?

Posted on June 29, 2014 at 22:48Many years ago i asked here if ST will do STM32 in other packages like DIP , SOnow i ask again. It would be very nice to have a F401 in a SO16 for instance.MKE04Z8VWJ4 is available in SO and NXP have 8pin DIP's!

STM32F373RC TTa output driving circuit

Posted on June 30, 2014 at 17:42Hi all, I would like to know where can i find the internal driving circuit schematics of a TTa output pin (PA0, pin 14) for the  STM32F373RC controller. PS: I think i might be an open collector with an internal pull u...

bmanogna by Associate
  • 1150 Views
  • 2 replies
  • 0 kudos

interrupt of the timer

Posted on June 30, 2014 at 02:32Can I have a link or an code example to count the rising edges that have an input signal in a prefixed time?I need the number of rising edges in a second.The frequency of the signal on a gpio input is in a range from ...

cchechio by Associate II
  • 1773 Views
  • 4 replies
  • 0 kudos

STM32CUBE + FreeRTOS + RTC HardFault

Posted on June 27, 2014 at 04:04Hi Everyone,I have the stm32f4dicscovery and built a simple project with STM32CubeMX 4.3.  I have attached the IOC file.  The code starts a task thread and blinks an LED.  The program hard faults when the RTC Init fun...

How to update the bootloader

Posted on June 30, 2014 at 11:17I have developed my own proprietary bootloader for STM32407 that work over UART and Ethernet. I can update the the application by the bootloader now.If I also want to , how can I realize it?

Resolved! STM32 nucleo-053 - USART issue

Posted on June 11, 2014 at 23:06Hi, I am familiar with Standard Pheripheral Library on STM32F100 MCU. ==== The problem is that on nucleo-053 (SPL is not available for this MCU) I cannot make USART working properly. I generated the code using CubeMX ...

Pa2 and Pa3 pins not working in stm32f030

Posted on June 30, 2014 at 07:25I have configured simple USART transmit and receive interrupt....It is working fine with othe pins for e.g PB6 and PB7.....but if I used Pa2 and Pa3 it's is neither transmitting nor receiving....What may be the proble...

sanjib by Associate III
  • 1232 Views
  • 3 replies
  • 0 kudos