STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 Standby Consumption

Posted on July 14, 2015 at 09:27 Hello, I am working on an application in which we rely heavily on the standby mode for maintaining battery life, but we're having trouble properly entering the standby mode. The CPU gets reset as it should...

jesper2 by Associate II
  • 1815 Views
  • 5 replies
  • 0 kudos

Disabling PWM at logic high

Posted on March 12, 2014 at 12:05 Hi , I am trying to disable my PWM with the pin at LOW when disabled however it seems to be always at HIGH. RCC_APB1PeriphClockCmd(TIM3, ENABLE); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;...

DMA data from ADC does not refresh

Posted on July 21, 2015 at 14:44Hello all,I am writing an application on a STM32F4 which reads from two sensors. I do it with two ADC3 channels with DMA. I use HAL_DRIVERSI write on a buffer several readings from three sensors by calling:HAL_ADC_Sta...

jmiguelg by Associate
  • 994 Views
  • 1 replies
  • 0 kudos

I2C NAK stopping SysTick

Posted on July 22, 2015 at 07:35Hi there, I'm trying to do a blocking I2C read in another interrupt. If I receive a NAK the HAL seems to crash (I'm seeing uwTick stop). Both the I2C interrupt and the interrupt I'm doing the read from have a lower (h...

0690X00000605IAQAY.png

STM32F3Discovery I2C EEPROM not working

Posted on June 16, 2015 at 02:56 Greetings. I am trying to use STM32F3Discovery(STM32F303VCT6)I2C interface to communicate with24C04 EEPROM device. And as for now all my attempts failed I've decided to ask for help. I initialize I2C1, then ...

Help with Stm32f429 FMC SDRAM(MT48LC16M)

Posted on July 21, 2015 at 17:15I design a board based on Stm32f429-discovery and add a 8192 Row x 512column x 16 bit Sdram to Sdram Bank 2. my Sdram is MT48LC16Mhttp://pdf.datasheetarchive.com/datasheetsmain/Datasheets-19/DSA-364195.pdf I study Dat...

High speed data transfer to STM32F3

Posted on July 20, 2015 at 23:34Hi All,I need to transfer a large amount of binary data to my STM32 and am trying to figure out what the best way to do this would be. The data throughput needs to be roughly 8Mbps. The device has USB so I was thinkin...

daniel2 by Associate II
  • 1884 Views
  • 3 replies
  • 0 kudos

Extra Data Transferred by DMA

Posted on July 21, 2015 at 21:27 Hi All, I'm configuring my DMA to transfer 48 bytes of data, and am triggering the DMA interrupt both on TC and HT events. Currently if I disable the DMA after the first interrupt, so I would expect to see...

daniel2 by Associate II
  • 2048 Views
  • 3 replies
  • 0 kudos

STM32F4 USB minimum operating voltage

Posted on July 21, 2015 at 22:20I am running the stm32f407 at 1.85V and was wondering if it would be possible to get USB working at this operating voltage. I've pulled up the d+ line to Vbus but cannot get proper enumeration. I believe as long as th...

gradoj by Associate
  • 1357 Views
  • 2 replies
  • 0 kudos

STM32F7xx I2C bus frequency too high

Posted on July 21, 2015 at 20:51Hello folks,I am working with an STM32F7 Discovery board which uses an STM32F746NG microcontroller.I would like to use the I2C peripheral without using the STM32Cube HAL, just by directly accessing the registers.I man...

joel23 by Associate II
  • 2014 Views
  • 2 replies
  • 0 kudos