STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SWD floats, STM32F2, code don't run

Posted on August 13, 2015 at 08:391. I am using STM32F205, with serial wire debug, composing reset, clk, data & gnd pins.2. Whenever I connect debugger my code runs perfectly. But without debugger, sometimes code just don't run. I am toggling a pin ...

How to read image file from SD card and display on LCD

Posted on August 07, 2015 at 08:45Hi,I am using STM32F103ZET6 development board interfaced with micro SD card. I am able to read and write data to the text file created in SD card using FAFTS but unable to read and display images stored in SD card o...

STM32F427 USART FIFO ?

Posted on August 21, 2015 at 23:48  Is there a hardware FIFO for USART6 and if so what size in bytes ? If not, example code of putting a FIFO in the interrupt handler ? How about the other USARTs and UARTs, do they have hardware FIFO ?

doreen by Associate II
  • 887 Views
  • 1 replies
  • 0 kudos

STM32 library: What is the best?

Posted on August 21, 2015 at 22:35Hello to all the forum,i'm new to the STM32 platform, i have buy the STM32F4 discovery board, and i have started some basic test with Eclipse and GCC for ARM.I have started my work with the HAL library, with success...

roberto23 by Associate II
  • 1607 Views
  • 2 replies
  • 0 kudos

ST-Link Utility External Loader sources

Posted on August 20, 2015 at 21:55Hello! I have custom board with STM32F746NG, sdram and NOR flash Spansion S29GL128S10 mapped at 0x6000 0000. I tried to download bin file into nor using external loader (used STM32F756G-EVAL) M29W128GL looks very s...

lukasz589 by Associate II
  • 2254 Views
  • 4 replies
  • 0 kudos

stm32f0 rtc

Posted on August 21, 2015 at 15:29 I downloaded application note write code.my device(stm32f0discovery,stm32f051r8t6).the weird thing with cube generated code it doesnt work either.In addition if I put breakpoint on while loop when I look rtc I s...

aaslan by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

VBUS fireworks ( STM32F407 drawing 50ma over PA9 )

Posted on August 18, 2015 at 14:50Hi all,in another Thread it is mentioned and confirmed that bootloader v2.0 will configure the stm32f105/7 devices usart1 in a way that vbus detection pin pa9 will draw about 45ma. ( /public/STe2ecommunities/mcu/Lis...

STM32F4 Input Capture TIM2 Channel 4

Posted on August 21, 2015 at 14:02Hello I'm faced to the Problem that I do have to use TIM2 channel 4 for Input capture. I know that channel 4 can not be used like 1 to 3. But I thaught I can use the channel 4 to get edges and take CCR4 as counter t...

oli by Associate II
  • 1266 Views
  • 1 replies
  • 0 kudos

STM32CubeMX freezes when generating code

Posted on August 11, 2015 at 10:26Hi,STMCubeMX is freezing every time I try to generate code for an STM32F429 project.  This is my first time using it, but everything so far has been pretty straightforward, and I haven't given it any crazy parameter...

njansen1 by Associate II
  • 3936 Views
  • 6 replies
  • 0 kudos

NOKIA LCD_6610 wrong STM32F107

Posted on August 21, 2015 at 16:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

aubin by Associate II
  • 826 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.