STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube improve config parameter UI

Posted on August 06, 2015 at 02:56Having to enable the description of the config parameters at the bottom of the window is non-sense.  there is plenty of room to add these in columns without taking any more space and will make it easier to browse fo...

ETM Trace on STM32F429

Posted on August 21, 2015 at 09:26Hello,I wanted to know if someone has already worked on ETM trace on STM32 cortex-M4. My purpose is to activate them into the embedded software itself and dumping traces on the 5 following pins (TRACED[0-3] + TRACEC...

STM32 ADC1 regular + ADC2 and ADC3 in injected mode

Posted on August 24, 2015 at 22:57Hi All,I've some problem configuring the ADCs of a STM32F407.I have 2 motors connected to my board that I drive with 2 different pwm.For the 1st motor I use a pwm from PE9 (TIM1 CH1)For the 2nd motor I use a pwm fro...

canta76 by Associate II
  • 1856 Views
  • 3 replies
  • 0 kudos

STM32F042 SWD IDCODE error

Posted on August 22, 2015 at 21:51I have a problem with debugging an STM32F042 board. When the debugger (ST Nucleo) asks for IDCODE, the MCU responds with an error (trace shown below). At first, I thought that the bootloader is the problem, so I fla...

0690X00000605IdQAI.png
atx by Associate II
  • 1081 Views
  • 2 replies
  • 0 kudos

Display orientation in STemWin526

Posted on August 24, 2015 at 21:17Hello!I need help.I need to use vertical orientation of display.I use demonstration from STM32F429I-Discovery.I try to use combination #define COLOR_CONVERSION_0 GUICC_M565 #define DISPLAY_DRIVER_0   GUIDRV_LIN_OSY_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.