STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 CAN in slave mode. Is it possible?

Posted on January 19, 2015 at 07:42Hello everyone! Help me, please. I've got STM32F042K6T6. Can I use it in an endpoint device? Here is only CAN interface, is it possible to use it as slave? Thanks! #slave #bxcan #stm32f0 #slave #bus #can #can

serkodog by Associate II
  • 3209 Views
  • 7 replies
  • 0 kudos

[Bug] STM32CubeMX, SAI->xSLOTR, SLOTEN not shifted

Posted on January 20, 2016 at 13:50 After spending an entire morning figuring out why my SAI configuration isn't working anymore I guess I found a new bug concerning the configuration of the SLOTR register inside HAL_SAI_Init. Prior to 1...

CubeMX and ADC Synchronous / 2

Posted on January 19, 2016 at 19:15Device:  STM32F030F4P  20 PinTool:  STM32CubeMX Version 4.12Using 8 Mhz external Crystal.  I arbitrarily set the clock configuration so that the APB1 Peripheral clock to 3 Mhz.Using ADC 1,4,6,7  -- On the configura...

STM32F746G-DISCO, STemWin, GUI_ANIM_HANDLE

Posted on January 19, 2016 at 20:22Hello. I'm testing STM32F7 discovery. The library is STemWin 5.28. I try to test WeatherForecast (the example form the Segger web site). The compiller gives a lot of errors concerning animation. Is it not included ...

baev_al by Associate III
  • 948 Views
  • 1 replies
  • 0 kudos

[F103] RTC_ALR not preserved after reset

Posted on January 21, 2016 at 01:03I have a problem with RTC_ALR behaviour. The RM0008 in 18.3.2 says:All system registers are asynchronously reset by a System Reset or Power Reset, except for RTC_PRL, RTC_ALR, RTC_CNT, and RTC_DIV.  The RTC_PRL, RT...

ziutek by Associate
  • 937 Views
  • 1 replies
  • 0 kudos

STM32 CAN Filtering

Posted on January 20, 2016 at 01:53 Hello! I have configured my filter banks. However, the standard ID that the receive FIFO0 register is reading after controller transmits a response to my module is not what I expect. Hence, I suspect t...

akshayamk by Associate II
  • 1796 Views
  • 2 replies
  • 0 kudos

How to read code from the device?

Posted on January 20, 2016 at 20:29I tried to read the code, binary data, from a Discovery Card F407 but noticed I can't. I tried ST Link and Keil. What is the problem? Surely this is not the first time some one wants to do this.

LMI2 by Lead
  • 1560 Views
  • 3 replies
  • 0 kudos

STM32CubeMX 4.12.0 bad code generated in stm32f4xx_it.c

Posted on January 06, 2016 at 13:58 void NMI_Handler(void) { /* USER CODE BEGIN NonMaskableInt_IRQn 0 */ /* USER CODE END NonMaskableInt_IRQn 0 */ HAL_RCC_NMI_IRQHandler /* USER CODE BEGIN NonMaskableInt_IRQn 1 */ /* USER CODE END NonMaskableInt_IR...

hbarta2 by Associate III
  • 1049 Views
  • 2 replies
  • 0 kudos