STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7xx Flash interface selection (AXIM or ITCM)

Posted on March 28, 2016 at 18:28I am confused about the boot setting in STM32F7xx series.When the boot pin is low, it boots from flash on ITCM interface (0x0020 000) by default, as shown in the screenshot of the manual.However, in the IAR linker fi...

0690X000006038MQAQ.jpg 0690X00000602vZQAQ.jpg
wenbin by Associate II
  • 6229 Views
  • 10 replies
  • 0 kudos

Parser advice with ISR

Posted on March 29, 2016 at 11:27Hi everybody.I am writing a program which, among the others, makes an stm32f427 mcu communicate with a GNSS module via SPI. The envinronment, further, consists of freeRTOS and the ST HALs. So far, I have written a mo...

valerio2 by Associate II
  • 704 Views
  • 0 replies
  • 0 kudos

USB on STM32F411RE

Posted on March 29, 2016 at 10:57Hi,I'm using http://www.st.com/web/en/catalog/tools/PF260320 to manage a printer trough a usb connection. I would to be sure that my usb connection is right.Pins connection :  Printer side STM32 side   Vbus 5V (r...

0690X000006034pQAA.jpg

WWDG EWI interrupt Issue

Posted on March 28, 2016 at 17:57Hi all,I have a serious issue with the EWI (Early wakeup interrupt) of the WWDG.I'm using STM32F103 and I'm based on the example of the firmware libraries, I add the configuration of the EWI interrupt : the source co...

JEN by Associate II
  • 1923 Views
  • 2 replies
  • 0 kudos

STM32F103 Does not RESET on Power Reset

Posted on March 26, 2016 at 09:46Dear All, I am facing a very strange problem in STM32F103RET6. It is showing completely random behavior on Power Reset. On some PCBs it RESET on every power Reset, while both PCBs have same hardware(means identical h...

STM32F3 12bit DAC with DMA - issue

Posted on March 28, 2016 at 09:59 Hello everyone, this is my first post on the forums. I've been following the posts for awhile and now I have myself faced a problem I can't seem to fix. I'm using a NUCLEO-F334R8 evaluation board and HAL ...

lkaino by Associate II
  • 1895 Views
  • 3 replies
  • 0 kudos

stm32f769 maximum dsi resolution

Posted on March 25, 2016 at 14:39Hello! I want to connect tft display with 1280*720 resolution via DSI interface. TFT panel has 4 differential inputs for data. There is no reference manual for stm32f769 controller on this page http://www.st.com/web/...