STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bi-directional Parallel ports

Posted on May 06, 2016 at 16:14Short question: What is the recommended way to implement a bi-directional data bus on STM32 using the HAL? Longer version: Our code needs to interface to a LCD controller over a 8-bit bi-directional bus. To do this, we...

Stm32f103 nucleo board with cubemx, variable pwm out

Posted on May 03, 2016 at 19:53hello im working with a nucleof103 and the cubeMX HAL library. i managed so far to get a steady pwm out via tim3_ch1 on PA6. but id like to change the DC after each periode, therefore enable interrupts and change then...

aal1 by Associate II
  • 1401 Views
  • 2 replies
  • 0 kudos

Issues with interrupt driven SPI DMA Rx

Posted on May 05, 2016 at 23:59 Hi, I'm trying to get an STM32F0 read incoming data packets as a SPI slave using the DMA. I've been reading the DataExchangeDMA peripheral example code and trying to convert some of it to an interrupt driven model...

0690X00000605NsQAI.png
banks2 by Associate
  • 2388 Views
  • 2 replies
  • 0 kudos

AN2606 System memory boot mode - Jumping to bootloader

Posted on May 05, 2016 at 17:39I am using a stm32f4discovery. When SB18 is removed (underside) to make boot0=1, to boot from system-bootloader, my windows7 sucessfully detects the USB DFU interface (it appears in Device manager in the ''Universal Se...

STM32F072 - Encoder, get velocity

Posted on May 06, 2016 at 15:21Hello,I have configured the encoder and it is working. Now I want to get the velocity so I need to configure another timer and capture the time of a encoder pulse. I can do this by software on interruptions but there i...

ee06091 by Associate III
  • 685 Views
  • 0 replies
  • 0 kudos

STM32 HAL CAN Tx Mailboxes

Posted on May 05, 2016 at 23:17Hi,I'm working on a project that uses the STM32 HAL drivers, and in particular the CAN driver in interrupt mode. I understand that the STM32F407xx microcontroller has three CAN transmit mailboxes, allowing users to ''e...

snavonne by Associate
  • 1596 Views
  • 1 replies
  • 0 kudos

USART2 Only Receives While Stepping in Debugger

Posted on May 06, 2016 at 00:01Hi, Set up on USART2 on STM32F4 Discovery board. Using PA2, PA3. I'm using Teraterm with a USB to serial adapter at 115200. After configuration, I send a string from the STM32F4 (''Hello\r'') which I see on the termina...

STM32 and STMPE1801

Posted on May 05, 2016 at 21:50 Hello. I try to set up STMPE, using the bus I2C. I need to control a LED, and the high level on GPIO5 pin is for this purpose necessary. I do setup here so: data_i2c[0] = CHIP_ID_REG; ...

mak1308 by Associate III
  • 530 Views
  • 0 replies
  • 0 kudos

STM32L052 StopMode high current

Posted on May 05, 2016 at 19:50Hi! I am using example from CubeMX FW L0 version 1.5.0 PWR/STOP MODE with RTC. I have STM32L052K8 revision Y. Current RUN/STOP = 11/6 mA (!). Where is uA??? I do'nt know. In readme file this example for: ''This example...