STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART only receive one data.

Posted on June 27, 2016 at 04:21Hello, I use STM32F303 Discovery board and try to test UART port.However, although I sent 5 sets of data, but the receiver port just only receive the first data. Does anyone know how to fix this issues?

yang2 by Associate III
  • 592 Views
  • 1 replies
  • 0 kudos

ADC with DMA triggered by software

Posted on June 22, 2016 at 15:32Hi,I would like to trigger the ADC conversion with DMA via a software command. I tried several configurations but I haven't succeed yet. The simplest thing would be to push a button and the ADC starts converting and a...

smrtkai by Senior
  • 3276 Views
  • 5 replies
  • 0 kudos

stm32f746-discovery

Posted on June 27, 2016 at 10:03Hello, I have a question about the demonstration code of stm32f746-discovery board. I can't see, in which file are defined the coordinates of touch buttons? #stm32f746-discovery

Suddenly - ST-Link Has Stopped Working !

Posted on June 26, 2016 at 17:50I have a problem here that doesn't make one shred of sense. I have boards (STm32F405VG) I programmed a couple months back that were fine. Meaning, I could connect to the board, and print the output statements from the...

EEPROM Emulation

Posted on June 26, 2016 at 11:59Can we interface external EEPROM with STM32f427 ? if yes can anyone please refer me some application note for STM32F427. I found AN3969 but it is for STM32f40x/stm32f41x and i need for STM32F427.

No ST-LINK detected

Posted on June 26, 2016 at 16:49Hello,I have a prototype board with:CP2102 USB - UART portSTM32F103RB(BOOT0 pin is configured highBOOT1 pin is configured low)Now I try to download some code to the board with Keil uVision.If I try to do it, the progr...

AHB transaction size

Posted on June 26, 2016 at 10:39i want to interface stm32f427 with 16 bit data bus external memories how can i change AHB transaction size to 16 bit ?

STM32F107 - mass storage device

Posted on June 17, 2016 at 11:06Hello,I am planning to build a device with a STM32F107, The user should be able connect to the system via both Ethernet and USB.When connected via ethernet, I should inform the IP address of STM32F107 to the user.For ...

rtursen by Associate II
  • 2604 Views
  • 8 replies
  • 0 kudos

STM32F437VIT6 = 168 MHz or 180 MHz ?

Posted on June 26, 2016 at 04:45We are looking at the STM32F437VIT6 and in the datasheet is saying the part has a max CPU frequency of 180MHz. I wanted to verify that the 180MHz was correct.When I checked the distributors online the part is listed a...