STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Works only after restart.

Posted on July 10, 2016 at 05:05Hi, I am new here so bare with me. When I start the device it wont run. And then when I hit the restart button it works. It also works perfectly in debugg. So I have no idea why this is happening. It is a self made PC...

0690X00000605QSQAY.png 0690X00000605BeQAI.png 0690X00000605QXQAY.png 0690X00000605NPQAY.png

Sample Rate Distortion/Aliasing on ADCs

Posted on July 09, 2016 at 00:17Hi, I am doing some audio programming on the STM32F4 and I am noticing that there is some distortion/aliasing happening around the sample rate. I was writing a program that reads the incoming audio into a delay buffer...

epalaima by Associate II
  • 1334 Views
  • 2 replies
  • 0 kudos

DMA Configuration for Multiple ADC Channels STM32F4

Posted on July 07, 2016 at 22:37Hi, I was wondering how I would go about configuring direct memory access for multiple channels of an ADC on the STM32F4. I have each individual ADC configured for DMA access currently but only with one channel each. ...

epalaima by Associate II
  • 2058 Views
  • 2 replies
  • 0 kudos

STM32 Infrared receiver / transmitter

Posted on July 06, 2016 at 23:15I am looking to implement IR into a project and I'm wondering if anyone has any examples I could work from. I would prefer the IR receiver / transmitter be small and surface moutable, not through hole.Essentially I wo...

cradoumis by Associate II
  • 4232 Views
  • 4 replies
  • 0 kudos

STM32 Nucleo F411RE

Posted on July 07, 2016 at 14:19Hello Experts, I have bought 2 Nucleo F411RE boards and planning to connect them using I2C protocol. I want to run timer on slave and every 1 minute the slave sends some hex number. I want to display the hex code by c...

Interrupt conflict on PB11 PC11 pins

Posted on July 08, 2016 at 15:14Hi,I'm working on stm32f410RB Nucleo board and I have to set interrupt on pins PB11 and PC11 but on CubeMX project setting one pin exclude the other one interrupt, why?I have to configure it manually or is an hardware...

redcrow by Associate
  • 1533 Views
  • 2 replies
  • 0 kudos

STM32L152D ADC with DMA not working

Posted on July 08, 2016 at 11:49 Hello everyone, I am implementing some code forSTM32L152D-Eval Board using CubeMX; I set up one ADC channel (on pin PF10) with DMA transfer, but I don't get any data after starting the DMA: HAL_ADC_...

anio1491 by Associate II
  • 1267 Views
  • 1 replies
  • 0 kudos

Stm32f4 beginner qustions

Posted on July 05, 2016 at 07:54Hi, I am new to stm32f4 and just started picking up some basic skills on it. Hope you guys help me answer my doubts even though the questions I ask are very basic but it will really help me out. 1. Why do we need a ti...

what's the initial stack address of stm32?

Posted on July 08, 2016 at 09:44 Hi guys: I've alredy checked the .map file. I found the two STACK 0x2000c170 Section 2304 startup_stm32f10x_cl.o(STACK) __initial_sp 0x2000ca70 Data 0 startup_stm32f10x_cl.o(STACK) And i...

BeMercy by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos