STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK debug

Posted on November 05, 2016 at 04:49HiI have been using my F3discovery to build an application, which is now finished, so I designed a new user PCB and after assembling and running my application all went well, until I tried to start the debugger wi...

kvresto by Senior
  • 1173 Views
  • 5 replies
  • 0 kudos

STM32F091RC IO toggle

Posted on November 06, 2016 at 14:58<p>Hello, I just started out with arm mcu's. I am using the Nucleo Board with the STM32F091RC mcu. </p><p>I encountered a problem that seems logically correct, however I receive no response from the board whatsoev...

Error during SystemClockConfig

Posted on November 06, 2016 at 16:34Hello Experts,I am using stm32L152VBTxA, STM32CubeMX, ST-Link/V2 and System Workbench for STM32.The Issue that I am facing is whenever I am writing a simple LED blinking code and running it using ST-Link/V2 debugg...

STM32F103RD GPIOC pin 2 default state errata

Posted on November 04, 2016 at 16:48While debugging an issue I discovered that on the STM32F103RD/VD silicon, GPIOC pin 2 defaults to SET/1 in the ODR.  All other GPIO ports default to RESET/0.  While it is always good practice to explicitly set the...

ggiger by Associate
  • 918 Views
  • 2 replies
  • 0 kudos

STM32F042

Posted on November 06, 2016 at 14:00Hi I have designed my first PCB ever so.My board has MCU STM32F042 and is based on nucleo reference design but for some reason I can not connect my stlink to using a nucleo stlink module in ''stand alone mode''.It...

F767 EMAC Debugging Suggestions

Posted on October 30, 2016 at 02:22Hi,I'm attempting to bring up LWIP under FreeRTOS for an F767 on a Nucleo board. I'm using code generated by Cube. This is my third STM32 project and I'm very comfortable using an RTOS but I am just becoming acquai...

kenny by Associate II
  • 1388 Views
  • 2 replies
  • 0 kudos