STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EWUPx and Stm32F412

Posted on January 31, 2017 at 13:49Hello,while DocID027813 Rev 4 chapter 5.4.2 knows aboit EWUP1..3, e.g.* @file stm32f412zx.h * @author MCD Application Team * @version V2.6.0only knows EWUP.EWUPx should be added in other headers too, where applicab...

stm32L476 12 Bit ADCs causing Spikes in Data

Posted on January 30, 2017 at 19:29Hi there,I am using the Stm 32L476 and I am trying to use 2 ADCs with 2 channels each with 12 Bit. So 4 Channels all together. I am using the ADCs in Regular simultanuous  multimode with DMA so I am able to transmi...

Bene Sch by Associate II
  • 3438 Views
  • 7 replies
  • 0 kudos

TIM3 Clock Frequence is ZERO

Posted on January 31, 2017 at 10:02Hi, everyone! I am writing code for a NucleoF303K8,using std periph lib . I am trying to output PWM via the D3 pin, which is PB0 of the chip. It doesn't work. So I try to find out what's wrong. But when checking th...

Li JW by Associate II
  • 2066 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F427 DFU-Mode

Posted on January 31, 2017 at 08:21Hello,I try to implement a bootloader via dfu mode.In my applicationi write a magic value and perform a reset.In the bootlaoder i read the magic value and try to jump to the system memory.Therefore i try this:Bootl...

uart interrupt, LowPower_Handler

Posted on January 31, 2017 at 08:23Hi.I am testing the I-CUBE-LRWAN(LoRa) Pingpong sample code.I am also testing uart interrupts.If you do not call the LowPower_Handler function in the main loop, the uart interrupt will work fine.However, calling th...

STM32f4 HAL_UART_RXit

Posted on January 30, 2017 at 13:46Hello everyone I am trying to use Interrupt based uart. I am facing problems to transmit and receive data continuously. i have attached the code.please can anyone help 

daynial by Associate II
  • 1494 Views
  • 2 replies
  • 0 kudos

Resolved! CubeMX v4.19.0: Can't Find Nucleo-F767ZI

Posted on January 27, 2017 at 05:03So I just installed v4.19.0 and now at the Nucleo-F767ZI is missing from the Boards List. (Just F746ZG and F722ZE are  there.) Prior to the install it was there and kinda worked but now it's not on the list.What am...

phroggie by Associate II
  • 3704 Views
  • 7 replies
  • 0 kudos