STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F413VG FSMC Muxed or Non-Muxed?

Posted on February 22, 2017 at 10:52I want to control several FPGA registers by FSMC bus. It's about 30 registers in the FPGA, each register 16bits.MCU package is LQFP100. STM32CubeMX makes the FSMC bus 3 options: LCD ; Muxed NOR Flash; Muxed PSRAM ...

0690X00000603abQAA.jpg 0690X00000603dPQAQ.jpg 0690X00000603dUQAQ.jpg

How to run custom bootloader...?

Posted on March 10, 2017 at 10:43Hi ,I'm writing one custom  bootloader which sits on top of actual serial bootloader . when I pull boot0 to low my custom booloader should run instead of running main application. Please give me some suggestions for ...

sudhan j by Associate II
  • 1290 Views
  • 2 replies
  • 0 kudos

QuadSPI with STM32L4 and Micron-QSPI-Flash

Posted on December 22, 2016 at 14:38I use a STM32L4 with a Micron N25Q032A (32 Mbit, 4Mx8). I have some Questions about this or similar Micron-Chips and hope to get here some Hints. After a PageWrite (Command 0x12 QUAD_IN_FAST_PROG) you have to pol...

Nor Sch by Associate III
  • 2829 Views
  • 4 replies
  • 0 kudos

UART AND STOP1 MODE

Posted on March 08, 2017 at 17:10I'm developping an application based on STM32L475. In this application I'm controlling a device that is managed via UART2 interface with AT commands. This device is correctly working in run mode but problem comes whe...

Resolved! STM32F3 Motor Timer Idle Setting / MOE Bit HAL Problems

Posted on March 09, 2017 at 17:00 I'm currently working on a Motor Controller using the STM32F3. I need the ability to start and stop the motors and, in particular, the ability to switch from moving to stopped and free-wheeling. It would seem tha...