STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to set LWIP debug to usart2 ?

Posted on July 24, 2017 at 10:29Hi,i already have done the setup for the lwip stack on the STM3210C-Eval board. I can already send via TCP/UDP and also RS232 to the uC (PC-->uC) and get also a echo back (uC-->PC). The debug output of the lwip-stack ...

HAL_CAN_Transmit timeout on STM32F429 using CubeF4 example

Posted on October 05, 2016 at 23:30 I'm having trouble implementing the STM32CubeF4 CAN example on my STM32F429I-Disco board. I'm using the CAN Network example provided with the STM324x9_Eval which in the readme.txt says: This example runs on STM32F...

16513584 by Associate II
  • 2442 Views
  • 5 replies
  • 0 kudos

Resolved! STM Flash Loader support for STM32F423 CPU missing

Posted on July 24, 2017 at 20:37Hello,The current version 2.8.0, and the pre-release version V2.9.0RC4 floating around in the forum, do not support the STM32F423 CPU. There is no map file for this CPU. Is there an updated pre-release of the program ...

STM32F303 Vih specification

Posted on July 26, 2017 at 03:40Data sheet for STM32F303 Vih specification indicates;1. TC and TTa I/O = 0.445*VDD + 0.3982.  FT and FTf  I/O =  0.5*VDD  + 0.23.  All I/Os except BOOT0 = 0.7*VDD.  Item 3 seems to contradict  1 and 2. Can this be cla...

D S by Associate
  • 1298 Views
  • 2 replies
  • 0 kudos

Resolved! RM0090: USART minimum attainable baudrate

Posted on June 29, 2017 at 17:15The mantissa in USART_BRR is 12-bit i.e. its maximum value is 4095. That limits accordingly the minimum attainable baudrate for given APB frequency.The following values in example tables are thus invalid and those bau...

0690X00000607WEQAY.png

STM32L4 SPI Clock phase

Posted on July 26, 2017 at 17:30Hi All, I'm using STM32L486RG microcontroler and 2 sensors using the same SPI interface (SPI1) I'm asking how to configure the SPI1 to communicate with 2 sensors when :  first sensor is working with SPI_PHASE_1EDGE s...

Resolved! STM32F407VG discovery kit read multiple encoder

Posted on July 25, 2017 at 18:04Hi all,I am try to use STM32F407VG discovery kit to read 5 encoder. I use TIM_HandleTypeDef and TIM_Encoder_InitTypeDef lib to read one encoder successfully. When I use the same code to read two encoders, I found that...

SWSTM32 Ac6 toolchain linker error

Posted on July 24, 2017 at 13:07Hi all,After building a project for the STM32F469xx processor I get a bunch of the following linker errors:<project_name>cubemx.elf uses VFP register arguments, <file_name>.o does not exist?failed to merge target spec...

Max Veen by Associate II
  • 1740 Views
  • 4 replies
  • 0 kudos

STM32cubeF7 project into atollic

Posted on January 27, 2017 at 03:24Hi All,I would like to import some of the STM32cubeF7 firmware package examples into atollic, but only sw4stm32 is supported. is there any way to solve this issue?Many thanksEsam

Raider E by Associate III
  • 1238 Views
  • 3 replies
  • 0 kudos