STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART 3 Receive Interrupt not working

Posted on August 04, 2017 at 15:48i have build with stm32cubemx usart 3 pc10 pc11 pin of stm32f446 115200,n,8,1 full duplex use with interrupt and receive interrupt not working all working fine if use alternate function uart4 on the same pin i think...

STM32F2xx Interfacing CMOS Image Sensor

Posted on August 07, 2017 at 07:17Hi,   Good day,   I an new in Image sensing technology.   Is 2752 x 2004 pixels image sensor can interface with STM32F2xx?   Waiting for reply.  Thanks in Advance.Nandish Jasani.

F446-429, core_cm4.h for NVIC setup?

Posted on August 06, 2017 at 03:26F446/F429Hi.Im trying to get NVIC work but it's very confusing, i dont do HAL/SPL.Are core_cm4.h all thats needed to setup and use NVIC?I basically need to get ADC1 to cause an interrupt so data can be processed.I t...

Resolved! CAN RX FIFO overflow handling in STM32F4 FW package V1.16.0

Posted on July 27, 2017 at 20:20Hiho,we recently updated one of our projects to the newest Firmware package and had to realize that receiving CAN Messages per Interrupt did not work reliably anymore. We were able to track the problem down to the fac...

Blacbird by Associate II
  • 3955 Views
  • 4 replies
  • 0 kudos

Problem with RTC

Posted on August 07, 2017 at 10:54HelloI have a problem that I can not solve.This applies to stm32f072. I need to make a check if the processor has been powerless for more than 200ms at boot time. Trying to use RTC and backup registry with milliseco...

STM32 MCO1/2 Driving a second chip XTAL input

Posted on August 07, 2017 at 06:36Hello all,In my project, I'm using the STM32F411CEU6, with a 9.6MHz External TCXO as a clock source. I would like to use the same clock to feed another chip in the board.I was thinking of using the MCO1 or 2 in orde...

0690X00000607s0QAA.png
meir3 by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

Is STM32 usable in this way?

Posted on July 13, 2017 at 12:49Dear sirs,I want to make drive recorder.I think to use, USB(Mass drive), SD card small, TFT window ,camera(I want many cameras).I do not want to make a proper product. I want only education or hobby.I found two produc...