STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB HID Barcode reader - keep disconnecting

Posted on August 15, 2017 at 12:27HiI have a USB barcode reader that acts as HID keyboard. When I plug it in to a Windows 10 machine it identified as 'USB keyboard device' (under device Manager - keyboards) and works fine: if I open text file and sc...

Y CS by Associate II
  • 1311 Views
  • 0 replies
  • 0 kudos

STM32f013RCT6 TIM4 PWM Output Error

Posted on August 15, 2017 at 07:55Hi,every,i want to use the TIM4 to output PWM signal,but the PB_6 always keep low.Here is the code:********************************************************************************************GPIO_InitTypeDef GPIO_In...

How to change from JTAG-DP to SW-DP (ARM Cortex-M4)

Posted on February 17, 2017 at 07:53Hello, Entering SW-DP mode can be done by following instructions in RM0351 chapter 44.3.1. External TCK/TMS sequence is required.Is there any other way to change from JTAG-DP to SW-DP? With ARM Cortex-M3 this can ...

Suggestions for Non-Blocking I2C Slave

Posted on August 15, 2017 at 02:33I'm using CubeMx with the STM32F415.Looking at the HAL drivers for I2C slave devices using DMA, it appears as if the HAL_I2C_Slave_Receive_DMA() and HAL_I2C_Slave_Transmit_DMA() functions will effectively be blockin...

STM32 libraries for newbie

Posted on August 14, 2017 at 11:47Hi,I am starting out with STM32 (STM32F103CB). I am thinking of using Visual Studio with VisualGDB and Seggar debugger. Are there high level libraries I can use for setting up IO functions and also for delays and no...

STM32F10x issue with SPI Master when reading

Posted on August 09, 2017 at 23:28 Hi, There seems to be an issue with the SPI peripheral in the STM32F10x family of devices. I have the same issue with multiple devices (STM32F103ZGT8, STM32F107VCT6) Here is the issue: When I try to ...

0690X00000607lcQAA.png

STM32L4 DAC DMA underrun error

Posted on August 12, 2017 at 17:43Hi guys,Iam trying to set up highest resolution on DAC as possible. If iam right there should be 10Msps DAC. so in 12b resolution i should get output samples 833 333.3ps. Timer (in my case TIM6) is clocked by intern...

marek2399 by Associate II
  • 1496 Views
  • 4 replies
  • 0 kudos