STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f042 CAN attempt

Posted on August 15, 2017 at 19:55Hello.I am using a stm32F042 for some CAN communications, alongside a SN65HVD230 as transceiver.I have two boards (my own) using both those ICs.I made a simple program, based on the STM32 example, from a STMCube ini...

Use CubeMX with BlueNRG-2

Posted on August 15, 2017 at 11:17Hi. Is it possible to use cubemx with BlueNRG-2? If yes how? Where to find code examples for this microcontroller, with interest for Bluetooth BLE. I want to start exploring this Upc and I needed information.Thank y...

A Bravos by Associate III
  • 1308 Views
  • 2 replies
  • 1 kudos

IAP problem - user app not working

Posted on August 15, 2017 at 14:11Hello. I am trying to implement an in application programming to an F303 processor.I got to a point where I can successfully download a whole new firmware to my desired location (0x08010000) through UART. I checked ...

VDD/VCORE Range 1 Voltages. 1.8V from 1.71V?

Posted on August 14, 2017 at 11:18Hi,Something is puzzling me. In the reference manual for the STML0x1 devices (Figure 11 and in other places) it states that, for Vcore Range 1, Vcore is regulated to 1.8V. It states that this is true for Vdd of 1.71...

nkatch by Associate II
  • 2979 Views
  • 4 replies
  • 0 kudos

How to read SFR

Posted on August 14, 2017 at 10:25Dear Sir:I am using STM32L476, and I have some issue on GPIO setting.If I only have BIN files, and I want see my SFR value, have any tools can do this?, flash my firmware and read SFR value.At this moment, I am usin...

Resolved! EXTI0 and EXTI1 not working PD0 and PD1

Posted on August 13, 2017 at 20:46Hello people,My design has buttons on the pins that are normally used for the system x-tal (PD0 and PD1) and a button on PC13.my MCU: stm32f103c8This is the code generated by cubeMx:<code>/** Configure pins as * An...

Hos by Associate II
  • 2627 Views
  • 2 replies
  • 0 kudos

renaming projects with SW4STM32

Posted on March 05, 2017 at 19:48I asked in their forums, but got no reply. Is there a recommended method for renaming a project in System Workbench (SW4STM32)? I tried just right clicking on the project name in Project Explorer and selecting 'Renam...

STM32H7 I2S_CKIN kernel clock

Posted on August 14, 2017 at 14:09Hi!Quick question about pin and I2S/SAI clock sources.If I wanted to use I2S_CLK pin (PC9) as kernel clock for I2S and SAI devices what is the recommended frequency in order to meet 44.1K and 48khz, 96Khz and 192Khz...