STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM Studio - only Array variables visible for F4?

Posted on February 15, 2017 at 06:52Hi,I am having a problem using STM Studio (version 3.5.1) - variables that are not arrays are not available to be imported and traced, while arrays are available. The problem is specific to the F4,  I have verifie...

stm32l476 External interrupt

Posted on March 07, 2018 at 09:15Hi,I am trying to use external interrupt.  I connect the PB3 to external output and I want to detect ricing voltage.I Using microcontroller STM32L476RG on Nucleo-L476RG.Moreover,I found the example that explained how...

Boris Fi by Associate
  • 1982 Views
  • 2 replies
  • 0 kudos

UART data transmit DMA problems

Posted on March 06, 2018 at 16:22Hello,i am working on a application where i try to measure a motor speed and current,  and then send the data to the PC using serial uart.The device used is a STM32F427For controlling the motor i used a timer1 6pwm c...

0690X00000609xBQAQ.png
Bogdan by Senior
  • 2000 Views
  • 4 replies
  • 0 kudos

USB HS Host BenchMarks

Posted on March 06, 2018 at 23:40Did any one test USB-HS Host throughput benchmarks for both Tx and Rx?In device mode i am getting around 120 Mbps (both tx and rx). Even STM replied that they are seeing the same speeds. But the results don't make se...

STM32CubeMX Makefile option.

Posted on March 06, 2018 at 23:19I recently upgraded my CubeMX from 4.18.0 to 4.24.0 and was  very pleased to see a new 'Makefile' option under Project->Settings->Toolchain/IDE.   I'd previously used SW4STM32 and then ran a python script to generate...

HAL UART_IT receive different length commands

Posted on March 06, 2018 at 19:03I am using the STM32F042F6 with ARM Keil toolchain. I am trying to use UART interrupts to receive commands of different lengths. I have managed to get it some what working using the attached code. I have made a recei...

STM32L475 flash reseted

Posted on March 06, 2018 at 17:55Hello,I'm working in my own prototype that is based on the STM32L475 device.Application is working fine: in this application, some data are saved into a reserved flash area. The problem I have found is that flash con...

SWP communication and still debug?

Posted on March 06, 2018 at 10:24 Hi I am using STM32L4 Nucleo board to develop an aplication which will be using the SWPMI port. I've been reading around and seems that the debug framework is already using it? So my question would be, how do I...

0690X0000060PGLQA2.gif