STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Powering up stm32

Posted on April 17, 2018 at 17:43which is best to power up    ''' STM32VLDISCOVERY '''   via 5V pins and a ground or 3,3V ???also which is best to for Digital Input for STM32VLDISCOVERY, using 5v or 3,3V ???In the data sheet I found that bouth of th...

Automatic re-join after reset or power-off

Posted on April 16, 2018 at 17:33Hi!Sorry but in Semtech Generic lora driver implementation, file MAIN.C , i need to connect the lora cube for call AT+JOIN and join OTAA network.I would like to automaticly join after reset or power off, also i think...

STM32F072RB CAN bus

Posted on April 18, 2018 at 07:17The original post was too long to process during our migration. Please click on the attachment to read the original post.

Nucleo L433RC-P UART Example

Posted on April 19, 2018 at 01:21Hi,I am new to the ST products and I am working with the STM32L433, I have an evaluation board. So, I was looking the software that you provide and for this MCU only have 5 examples. (PWR and Templates). I was wonder...

How does USB Host CDC data communication work?

Posted on April 18, 2018 at 02:11Hello everyone,I'm trying to get USB Host CDC working on STM32F407-DISC board. I'm using USB library version 2.2.0.So far, I got enumeration working fine by connecting a CDC device. I'm able to send data to the CDC d...

Pilot B by Associate II
  • 1425 Views
  • 3 replies
  • 0 kudos

nucleo F429ZI template

Posted on April 18, 2018 at 22:41Hello,I am new for STM32. I got NUCLEO-144 F429ZI board. it is pretty good start board. However, it seems pin mapping are different from different board. I can't find any documents to tell me the pin mapping. I use s...

yang hong by Associate III
  • 704 Views
  • 0 replies
  • 0 kudos

Re: port uclinux on stm32f7?

Posted on April 14, 2018 at 15:23I add earlyprintl support for stm32f767igt,and it seems success.i modified the start_kernel() function as belowextern void printascii(const char *);asmlinkage __visible void __init start_kernel(void){ char *command_l...

DFSDM and ADC

Posted on April 18, 2018 at 17:00Does anyone has been able to use DFSDM to filter data from the internal ADC?I have ADC triggered by a timer in order to acquire data equidistant in time.It works fine but I need to filter them better than using its o...

giuseppe by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos

Another question about HAL_UART_Receive_IT

Posted on April 18, 2018 at 15:01Recently, I've encountered problems with 'HAL_UART_Receive_IT()'. So I go here for solutions. I see several suggestions to put another 'HAL_UART_Receive_IT()' in  'HAL_UART_RxCpltCallback()', but they didn't give whi...

Slow SPI data transfer B-L475E-IOT01A kit

Posted on April 18, 2018 at 06:43HiAfter looong work with Microchip's PICs we are moving our desing on the fly to STM32L4 series MCU because it has hardware SDIO core. After some tests I see 55Mbps on STM32L476-EVAL with microSD Class 10 and 32KB bu...

0690X0000060AdIQAU.png 0690X0000060AdRQAU.png 0690X0000060AdNQAU.png 0690X0000060AdWQAU.png