STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_I2C_Mem_Read reads only correct if the parameter is wrong

Posted on September 24, 2014 at 13:18Hi,I have a STMCube generated project wirh I2C memory 24LC512 with following problem. The line:Status = HAL_I2C_Mem_Read(&hi2c1, IIC_ADDRESS+1, 0, I2C_MEMADD_SIZE_8BIT, pNVRawData, NVRawDataLen, 1000);is correct ...

Osto by Senior
  • 6838 Views
  • 11 replies
  • 0 kudos

where do I find libraries and support to connect touch tft

I see a lot tft on ebay and aliexpess which come with libraries and support for arduino and raspberry.I do not see anything for STM32. I am trying to get working 320 x 480. On arduino I had it working the next day, tons of sample programs and librar...

MNapi by Senior III
  • 1077 Views
  • 2 replies
  • 0 kudos

Resolved! How to initialize external SRAM in system_stm32l4xx.c

I am trying to initialize my external SRAM before the main loop runs. Using the STCubeMX it generated the code for me to have me FMC controller initialized after Hal_init() and Hal_GPIO_Init() in Main.c. However, I need the SRAM to be initialized bef...

NUCLEO-F303RE ADC interrupt issue?

Hello everyone,could someone please help with the following, I am trying to use ADC with interrupts. Doing the same thing with STM32F103C8T6 it works without issues, but using nucleo board it doesn't.Could someone please have a glance on the code ? (...

Resolved! Issue with PLL of the STM32F302

Hello, we're using the microcontroller STM32F302C8 and we have a problem with the PLL.The problem is when we enables the PLL the microcontroller is reset. We have made several tests using HSI and HSE, but always the same result, a reset after to enab...

GYacc by Associate II
  • 3068 Views
  • 4 replies
  • 0 kudos

STM32F746 Discovery default screen reset

I am new to Electronics and recently bought STM32F746 Discovery Board and connected to to my laptop using USB cable to STLink connector pin. Main screen light up showing programs pre save in it. and uploaded run LED blink code and then screen went of...

MMalv by Associate
  • 1357 Views
  • 1 replies
  • 1 kudos

Is the 4mA increase in current consumption expected when we just enable the wide bus operation in uSD card via SDMMC interface in STM32 MCU?

In a product which requires power consumption to be minimum as possible, we are employing a STM32L496 as MCU. In recent days, we were trying to bring down the power consumption of the overall device. We observed that immediately after enabling the wi...

HP.15 by Associate II
  • 1986 Views
  • 4 replies
  • 0 kudos