STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN STM32F303

I USED HAL_CAN_AddTxMessage FOR TRANSFER MESSSAGE BOUT I NEED KNOW WHEN THIS MESSAGE IS FINISH BEFOR START NEW MESSAGE

Resolved! Load program using Micro-B USB

Hello,I'm using STM32F030 series controller. currently we use JTAG connector to load a program into flash memory, using ST-LINK debugger externally.Now i want to load a program into flash memory using Micro-B USB in my device without using any extern...

SPraj.15 by Associate II
  • 2638 Views
  • 5 replies
  • 0 kudos

STM32F4: EXTI: Fails to capture rising edge interrupt sometimes

In out project we are making use of EXTI for interfacing a radio (RF) ASIC with STM32F411. Whenever, the radio has some data to be sent host it interrupts the host using the I/O line (drives the line high). This I/O line stays high till data is read ...

MSuhe by Associate III
  • 5831 Views
  • 15 replies
  • 0 kudos

STM32 USART synchronous mode receive does not work

Hello,I am using a STM32L052K6U6 to communicate with an SPI slave using the UART1 synchronous mode (configured with CubeMX, using the LL library).This is part of the code that receives data:while(!LL_USART_IsActiveFlag_TXE(USART1));LL_USART_TransmitD...

Fr4nky by Associate II
  • 3419 Views
  • 5 replies
  • 0 kudos

mcu halt when a Contactor is turned on

i have a an stm32f417vgt6 mcu and its connected with ft800 through 30 cm SPI cable and the ft800 is driving a tft lcd .. the problem is when the mcu turn on or turn off the Contactor the mcu halt .. can you please help me how to detect the prob...

How to measure 3phase L-L 440 volt using STM32 ADC?

i want to build circuit that can measure AC voltage 0-600V AC using STM32 it there any sample circuit and example code of it..i have try some circuit ...1) 0-400v ac --> stepdown transformer --> 0-15v ac --> dc --> resistor divider --> adc pin MCU b...

Resolved! Connect STM32F4 with smart card ISO7816

Hi, everybody. My task is to connect STM32F4 discovery Board with Smart Card ISO7816. I don't use interface ST8024CDR only hooked paid directly by the scheme specified in the image:I tried to adapt the Cubex project to STM32F1xx-EVAL. ATR reception d...

0690X000008ANWeQAO.png