STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a free to use STM32 simulator ?

I want to benchmark some code on a variety of STM32 devices before choosing the target device so would like to do this in a software simulation first. Are there any free or one-month trial simulators available that know all (most?) of the STM32 ran...

MikeDB by Lead
  • 2128 Views
  • 4 replies
  • 0 kudos

SYSCFG Clock STM32F4x

Hi!I am about to code my CLK enable tree, without CUBEMX. - I just took CUBEMX as referene.CUBEMX generates me a line called __HAL_RCC_SYSCFG_CLK_ENABLE(). Unfortunately i could not find any clock called SYSCFG in the clock tree (CubeMX nor DM31020)....

WalterE by Associate II
  • 3288 Views
  • 3 replies
  • 0 kudos

USART to USB /CP2102N/ Visu Tera Term

Hello,I visualize in a terminal Tera Term what comes out of the UART1 or UART3 or UART6 of a STM32F407VGTx via a Silabs CP2102N-based UART to USB module.Port and Terminal configurations matchThe connection is via the COM15 port. The TX / RX inputs / ...

CC_ROB by Associate II
  • 1175 Views
  • 0 replies
  • 0 kudos

GPRMC date ?

Dear MemberI tried to get date from GPRMC, but not getting any response:code :sscanf(str,"$GPRMC,%s,%2hhd%2hhd%2hhd,%c,%f,%c,%f,%c,%f,%c,%f,%f,%2hhd%2hhd%2hhd,%f,%c,%c,*%2s\r\n",&GPS.GPRMC.xxRMC,&GPS.GPRMC.UTC_Hour,&GPS.GPRMC.UTC_Min,&GPS.GPRMC.UTC_S...

Flash Loader STM32H750

HI,I'm trying to create a Flash loader for ST-Link Utility or Cube-Programmer for STM32H750.I have successfully made the STM32F7 flash loaders, while with the STM32H7 I have the following problem:17:36:19 : Connected via SWD.17:36:19 : SWD Frequency ...

GGatt by Associate II
  • 1383 Views
  • 2 replies
  • 0 kudos

Resolved! How to flashSTM32F3 via UART1

Im new, hope this isnt dumb question. I have an erased STM32F303 and want to upload my code via UART1. I I have an FTDI USB to serial converter. I set BOOT0 pin=H and have the "Demonstrator" program for Windows working. Since the MCU is blank, how d...

Trich by Associate
  • 1801 Views
  • 3 replies
  • 0 kudos

Why the MCU hangs?

Dear friends,I am using STM32F107RCt6 MCU and I am running a TCP server on it using LwIP and freeRTOS.The total heap size of freeRTOS is 10KB and there are two tasks which each task has 256 wods stack. One task is used for Modbus TCP server and the o...

Mujtaba by Senior
  • 4246 Views
  • 10 replies
  • 0 kudos